// JavaScript Document
// This script controls the languages used on the flash pages.
// v $Revision: 1.1 $
// Created On: 05/01/08
// Modified On: $Date: 2009/02/06 13:04:41 $

var lang = document.gSearch.x.value;
var langCode;

// As new languages are needed, add the WCM numeric language id
// and the 3 letter langiage code as pairs to this array.
// A 3 LETTER CODE IS REQUIRED, ALL LOWERCASE!!!
var langCodes = new Array(["1", "jpn"], ["7", "eng"], ["8 ", "deu"], ["9", "esl"], ["11", "fra"], ["12", "por"], ["14", "swe"], ["15", "zho"], ["16", "vie"], ["17", "tha"], ["20", "ara"], ["48", "ind"], ["69", "nld"], ["70", "ita"], ["71", "nor"], ["72", "tur"], ["73", "ell"], ["74", "slv"], ["75", "hrv"], ["76", "mon"], ["97", "rus"], ["98", "bos"], ["99", "mkd"], ["100", "srp"], ["101", "sqi"], ["102", "por"], ["103", "kor"], ["104", "fin"], ["105", "dan"], ["333", "pol"], ["463", "zho"], ["464", "tam"], ["465", "hun"], ["511", "fra"], ["521", "may"], ["534", "spa"]);

for (i = 0; i < langCodes.length; i++) {

  if (langCodes[i][0] == lang) {

    langCode = langCodes[i][1];
  }
}

// If no language can be determined then default to english.
if (lang == null || langCode == null) {
	
  langCode = "eng";
}