Wastewater Treatment Plants: Utilizing Methane for Power Production
Many wastewater treatment operations use waste sewage gas from facility processes as a generator set fuel source. Comprised primarily of methane and carbon dioxide, the gas is generated by wastewater digesters used in the water treatment process, and captured to provide the plant with electricity and heat for the digester or other thermal loads. Benefits from methane-to-energy projects include:
- Increased energy efficiency
- Reduced electricity costs
- Decreased environmental impact
How It Works
Cat low-energy fuel generator sets are engineered to handle fuel with variations in methane content, which is typical of sewage gas. These specially designed generator sets also offer features to protect against moisture and the contaminants in sewage gas. They include:
- Crankcase ventilation pump to eject potentially acidic blow-by gases
- Specially designed aftercooler cores, cylinder heads, main bearings and connecting rod bearings that are hardened against corrosive elements
- Differentiated cooling systems to operate at elevated jacket water temperatures to prevent condensation of contaminants

United States / Canada [change]
Visit Caterpillar.com