Agriculture, Food Processing and Biofuel Manufacturing: Producing Electric Power from Biogas
- Reduce carbon emissions through the destruction of naturally occurring methane
- Reclaim valuable land space normally utilized for purifying organic wastewater
- Eliminate odor and pest issues caused by the decomposition of organic material
How It Works
Consisting primarily of methane and carbon dioxide, biogas is produced through the anaerobic decomposition of organic waste. Instead of allowing the organic waste to decompose in an uncontrolled setting, the waste and resulting gases are contained in an oxygen-deprived environment such as a covered lagoon or above ground steel tank. From there, methane is extracted and burned to generate electricity or heat.
Because of the impurities and inconsistencies in biogas, pretreatment is generally required. However, using a gas engine specifically designed to operate on biogas can reduce the amount of investment in pretreatment. Cat low-energy fuel generator sets are engineered to handle fuel with variations in methane content, which is typical of biogas. Cat biogas engine features include:
- Crankcase ventilation pump to eject potentially acidic blow-by gases
- Specially designed aftercooler cores, cylinder heads, main bearings and connecting rod bearings that are hardened against corrosive elements
- Differentiated cooling systems to operate at elevated jacket water temperatures to prevent condensation of contaminants

United States / Canada [change]
Visit Caterpillar.com