|
Cat C7.1 Engine with ACERT TechnologyThe C7.1 engine provides 168 kW (225 hp) at 2200 rpm with a torque of 872 N-m. The combination of large displacement and high torque allow the BG1000E to perform under the toughest conditions.
Cat C6.6 Engine with ACERT TechnologyThe C6.6 engine provides 168 kW (225 hp) at 2200 rpm with a torque of 1028 N-m. The combination of large displacement and high torque allow the BG1000E to perform under the toughest conditions.
Emissions Reduction TechnologyThe Cat C7.1 engine is equipped with a Diesel Particulate Filter (DPF) that traps soot from the
exhaust stream. The soot is removed through a process called regeneration, while the ash
remains in the filter and must be removed at a required service interval of 5000 hours. The C7.1
engine utilizes two types of regeneration, passive and active.
RegenerationRegeneration occurs during normal idle periods. The C7.1 utilizes two types of regeneration: active and passive. Neither active nor passive regeneration require operator intervention.
Meets U.S. EPA Tier 4 Interim and E.U. Stage IIIB Emissions StandardsReduces oxides of nitrogen by 50 percent from Tier 3/Stage IIIA levels. Reduces particulate matter by 90 percent from Tier 3/Stage IIIA levels. Ultra Low Sulfur Diesel (ULSD) fuel is required. Engine oil must meet Caterpillar ECF-3, API CJ-4/ACEA E9 specifications.
Service, Maintenance and RepairEasier service, maintenance and repair is accomplished by monitoring key functions and logging critical indicators. Advanced electronic diagnostic capabilities are possible using Cat Electronic Technician.
Eco-mode increases fuel efficiencyOnce activated, Eco-mode reduces engine rpm from 2200 rpm to 1650 rpm, which is suitable for most normal paving applications. The reduction of engine rpm during operation will reduce fuel burn compared with normal engine rpm. If an application demands more power, Eco-mode can be deactivated to return to 2200 rpm.
Cat C7.1 Engine with ACERT™ Technology ACERT Technology utilizes a series of Caterpillar engineered innovations that provide advanced electronic control, precise fuel delivery and refined air management. » Learn More
Fumes Management System The ventilation system draws fumes from the conveyor tunnel as well as the auger chamber and redirects them away from the operator for a more comfortable working environment.
Variable Speed FanThe variable speed fan is electronically controlled and hydraulically driven providing on-demand cooling, reduced engine power demand and quiet operation.
High Capacity Cooling System The high capacity cooling system allows the fan to run slower, reducing power demand while extending component life. » Learn More
Dual Operator StationsThe dual operator stations incorporate fully equipped consoles with adjustable suspension seats, armrests and retractable seat belts.
Operator VisibilityThe dual operator stations can be
positioned in one of four different
locations to provide optimum visibility. The stations can extend beyond the machine frame for good visibility when joint matching or while paving other applications where precise control is required.
Dual Operator Stations The dual operator stations provide complete control and good visibility from either side of the operating platform. » Learn More
Excellent MobilityThe sharp turning radius and high speeds allow the paver to move quickly around the job site.
Three Propel ModesPave, travel and maneuver modes provide good control and versatility. The maneuver mode provides less than a 0.5 m (1.5') inside turning radius for excellent maneuverability in tight quarters.
Large Drive TiresThe 18.00 R25 sand-rib drive tires provide good tractive effort and a smooth ride.
Large Steering TiresThe 16" x 22", solid rubber steering tires provide maximum ground contact and smooth operation.
Front SuspensionFour, front solid rubber steering wheels are mounted on pairs of oscillating bogies, providing a smooth ride.
Steering AssistSteering assist feature improves maneuverability and enhances component life by adjusting the drive speed of one side of the propel system according to the steering angle of the front wheels which allows the machine to turn while maintaining the same speed.
Front Wheel Assist (Optional)The front wheel assist feature provides power to the rear bogey wheels for additional tractive effort.
Long Wheel BaseThe long wheel base provides good tractive effort and stability on soft base materials.
Wheel Undercarriage System The wheel undercarriage system provides excellent mobility and maneuverability along with a smooth ride for optimum performance. » Learn More
Operator ConsolesEach operator’s station includes ground speed indicators, material handling controls, propel controls and screed extender controls. The controls for each station are in the same relative position providing easy control from either console.
Speed Control DialA speed control dial located on each operator station allows the operator to set a maximum travel speed which is important for producing a smooth, high-quality mat.
Machine ControllerThe machine controller integrates performance functions and allows the feeder and auger speeds to be set independently which extends component life.
Advisor DisplayThe Advisor display provides visual references, self diagnostics, and planning tools that keep the operator informed for better overall job site performance.
Operator Consoles The operator consoles are designed for productivity and accessibility. All gauges and displays are grouped for convenient and simple operation. » Learn More
Mix DeliveryThe BG1000E provides precise mix delivery with minimal operator monitoring through the most advanced material handling system.
Feeders Controlled IndependentlyLeft and right feeders in addition to the left and right augers are controlled independently. The ability to control these four components separately, through a machine controller, eliminates the need for feeder gates.
Mix Delivery ControlIn order to control mix delivery, the operator sets a speed rate for each feeder that will maintain the desired mix level in the left and right auger chambers.
Once the feeder speeds are set, the ratio of feeder speed to the maximum auger speed is automatically maintained by the machine controller, even though the propel rate may change as the job progresses.
Ratio ControlThis ratio control capability is particularly helpful when paving wider on one side of the machine than on the other. Each feeder can be set at a specified speed to deliver the proper amount of mix that is needed.
Exclusive Material Delivery System Productivity and quality enhancements are built-in features. » Learn More
Outboard Feeder Drives Increased live tunnel area provides easy servicing.
Gateless Feeders Run Full of MixThe gateless feeders on the BG1000E always run full of mix regardless of the speed required to fill the auger chamber. This is typically a slower speed than would be experienced with a paver utilizing feeder gates to control mix delivery rates. By not always having to run at full speed, feeder component wear is significantly reduced.
Changes in Feeder SpeedWhen changes in feeder speed are required, delivery of mix to the augers is immediate. This is in contrast to pavers with gates, where any delivery rate change is delayed for the length of time it takes to clear the tunnel of mix from the previous gate setting.
Running at Lower SpeedsRunning at slower speeds can also help reduce the opportunity for segregation, especially when working with larger stone mixes that have more of a tendency to segregate.
Gateless Feeders Variable speed feeders precisely control mix delivery while reducing wear and segregation. » Learn More
Feeder Design Tunnel construction improves mix flow.
Auger Assembly Provides mat consistency while minimizing segregation.
Single Control SwitchA single switch on the tractor’s operating console activates the generator. The generator operates at 1800 rpm and includes GFCI protection.
Generator System (Optional) The high capacity, integrated generator ensures peak performance and high reliability. » Learn More
Auxiliary Power Panel (Optional) The auxiliary power panel provides efficient power for night-time lighting and other job site power needs.
Operator-Friendly EnvironmentThe electric screed plate heating system eliminates the use of diesel fuel burners, creating a user-friendly environment.
Fast Warm-Up TimeThe electric screed provides a warm-up time in 30 minutes or less to 122° C (220° F) when ambient temperatures are at or above 22° C (40° F).
Proven and ReliableWhether you are paving interstates, highways, residential streets or commercial sites, the electric screed heat system performs under the toughest conditions.
Simple OperationThe screed control panel incorporates touch-pad technology with high intensity LEDs that promote simplified use and diagnostic capability with minimal operator training.
Multi-Zone Heating ElementsThe heating elements are mounted to the screed plates in a multi-zone configuration to provide even heat distribution.
Thermostatically ControlledThe screed plates incorporate thermostatically controlled temperature sensors in each screed section including the extenders. The temperature sensors provide inputs to the screed controller.
Electric Heat Screeds The AS3301C and AS2301C vibratory screeds, as well as the AS4251C and AS4252C tamper bar screeds feature multi-zone electric heating, easy-to-use touch pad interface, and even-heat distribution. » Learn More
Advisor DisplayThe Advisor display provides visual references, self diagnostics, and planning tools that keep the operator informed for better overall job site performance.
Large Access Doors and PanelsPreventative maintenance points can be accessed through the large swing-open access doors and panels.
Remote Lubrication PointsGrease fittings are grouped to provide quick, routine service of bearings.
Quick-Connect Sampling PortsThe quick-connect ports simplify retrieval of critical fluids for diagnosis.
Color-Coded and Numbered Electrical SystemTroubleshooting is efficient and simplified with the color-coded and numbered electrical system.
Electronic Control Modules (ECMs)The multiple ECMs communicate with
the Advisor display. The display lists service codes, providing quick reference. The ECMs are compatible with Cat Electronic Technician and easily connect to a laptop computer for fast technical support.
Serviceability Simplified service means more paving time and less maintenance time. Large swing-open doors and panels provide convenient access to service areas. Transverse engine mounting provides ground-level access to hydraulic pumps and the engine cooling system. Color-coded and numbered wiring simplifies troubleshooting of the electrical systems. The standard 500-hour engine oil change interval increases machine up-time. » Learn More
Propulsion ControlThe machine controller provides accurate control of steering and propulsion systems and ensures straight-line tracking.
Closed-Loop Hydrostatic Propel System The closed-loop system automatically compensates for component wear, hydraulic oil temperature and oil viscosity changes to ensure complete, low-effort, operator control. » Learn More
Project ConsultingProject consulting provides a service for improving smoothness, density, and productivity.
Technical TrainingTechnical training offers in-depth hands-on training to mechanics at Caterpillar training centers or customer locations.
Application TrainingPaving Operations Training (POT) is a hands-on methodical approach to the process of paving. The process of “Paving by the Numbers” guides the crew when setting up to pull off the joint.
Caterpillar Customer Support is Unmatched in the Industry Caterpillar offers “Solutions and Services” and around-the-clock support that meets your everyday needs. » Learn More
|