commercial generators for business

commercial business

Commercial Business

Power that works as hard as you do.

You’re trusted to power the places people work and to do it cost-effectively. Select a distributed generation system to provide power to a facility on a permanent or temporary basis or design a standby power plant. We even offer exhaust emissions for highly regulated emission environments, and utility grade Cat® paralleling switchgear so you can sell excess electricity to your local grid. Run uninterrupted power and reduce operating expenses with a Cat combined heat and power (CHP) system to simultaneously provide electricity for electrical loads and recover heat to warm facilities.

Our commercial generators offer world-class fuel efficiency and low life-cycle costs. Caterpillar is providing power to meet your demands and to help you cut costs with cogeneration technology. We’re here to keep power production efficient so you can focus on business.

Cat® Diesel Generators Supply Emergency Power to World's Tallest Data Center

Sabey Corporation developed Intergate.Manhattan into what is now the tallest data center in the world. Located in New York City, the facility presents a unique set of challenges including security, preservation and power loss. Sabey relies on its partnership with the local Cat® dealer, H.O. Penn, for emergency backup system support and critical data management.


Electric Power products

power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products

Customer Stories

São Paulo, Brazil — one of the fastest growing cities in the world — has the largest economy of all Latin American cities, measured by per capita GDP. To continue its fast-paced growth, the city must continue to have reliable sources of energy to feed the expanding commercial and industrial complexes being built.

View Customer Stories

Brochures

View our power generation brochures

Caterpillar offers standard and customized power solutions for all your applications, where you need it, whenever you need it.

View Brochures

White Paper

Caterpillar is pleased to provide information on new technologies as well as innovative solutions to power your business.

View White Papers

Reduced Operating Costs via CHP, Distributed Generation, and Standby Power

Many commercial businesses such as resorts, shopping malls, high-rise office buildings, universities, data centers, and hospitals, can reduce operating costs by implementing a Cat combined heat and power (CHP) system (also known as cogeneration) using clean pipeline natural gas as a fuel source. Cat® gas generator sets can simultaneously provide electricity for electrical loads and heat energy for a facility's thermal requirements. Benefits from CHP projects include:

  • Energy efficiency up to 90 percent
  • Reduced energy costs versus separate heat and electrical generation systems
  • Reduced emissions versus separate heat and electrical generation systems
  • Leadership in energy and environmental design (LEED) certification via energy efficiency credits
  • Where the capture and use of waste heat is not viable, your facility may still benefit financially via distributed generation (DG), where electricity is simply produced locally or via a natural gas fueled emergency standby power plant.

This is especially true when any of the following apply:

  • The local electric grid is unreliable
  • Natural gas is an inexpensive alternative to grid electricity
  • Reduced emissions versus separate heat and electrical generation systems
  • Generators can be applied during peak times of day to avoid high electrical utility demand charges (also known as peak shaving)

How CHP Works

Any Cat natural gas fueled engine can be configured for applications involving heat recovery. The engine drives a Cat generator to produce electricity, while jacket water and/or exhaust cooling circuits are fed through heat exchangers to transfer the waste heat from the engine to a your hot water or steam circuit. That hot water or steam can then be effectively used for the facility's process or HVAC requirements, including facility cooling when implementing an absorption or adsorption chiller (known also as trigeneration).

Caterpillar provides customized CHP packages, including the required mechanical equipment and controls to capture and transfer the engine thermal energy to your facility. Caterpillar also offers:

  • Natural gas fuel pressure regulation and safeties
  • Exhaust emissions aftertreatment for highly regulated emission environments
  • Utility grade paralleling switchgear to run multiple generators together or to export energy to the local electric grid
  • The total energy cost savings of such systems can more than offset the total owning and operating costs, delivering a payback in as little as two to three years, depending on local energy pricing and policies.

How Distributed Generation and Standby Power Work

When power is produced locally without heat recovery from the engine, Caterpillar provides radiators to provide proper cooling to the engine jacket water, engine oil, and aftercooler water circuits. Cat paralleling switchgear allows generators to operate with one another or in conjunction with a local utility power source.

Although diesel fueled emergency power systems will always be the solution of choice for life safety emergency standby systems, there has been an increasing move toward natural gas fueled standby power systems in recent years. Typically installed with an automatic transfer switch (ATS) or paralleling switchgear control for multiple generators, these systems sense when a utility outage occurs and automatically starts the backup power system and transfers power to the emergency source. When normal grid power returns, the control system automatically switches back and shuts down the emergency generator.

Cat® power stands up to Hurricane Sandy

When Hurricane Sandy made landfall, the Joint Meeting of Essex & Union Counties wastewater plant treated all the raw sewage that came into the facility during the storm. None of the treatment tanks overflowed, even when the nearby Elizabeth River and the Arthur Kill saltwater channel flowed in.

Learn More
Project Financing

No project is the same - from the application to the power need. That's why we offer a range of project financing options.

See our Offers
Precision Sizing at Your Fingertips.

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat® Electric Power SpecSizer.

Learn More
Electric Power Social Media

Check out the Cat® Electric Power social media page for the latest news, preventive maintenance tips, and product and show announcements.

Learn More
Cat® Dealer Service

The Cat dealer network is always ready to help. Find your dealer and read the latest in electric power service and support.

Get in touch today
Project Financing

No project is the same - from the application to the power need. That’s why we offer a range of project financing options.

See Our Offers
Electric Power News

Read the latest electric power news and articles relating to Cat electric power products by people in the know, on topics that matter to your business.

READ MORE