UTILITY POWER GENERATION

UTILITIES

Utilities

Exceptional power for the everyday.

You supply power to meet everyday needs, whether it’s peak shaving to save costs or off-grid power for isolated, remote cities. That's why you need a source runs non-stop — since life does too. Cat® stationary or temporary diesel generators are cost-effective, reliable power, meeting spikes in demand and keeping power affordable for your customers.

Your local Cat dealer is your source for on-going service and support. Our products and our team are working to power your world.

Power in the Jungle

Isolated from the national grid, 470,000 Brazilian residents were suffering frequent brownouts and power rationing. Critical action was needed to provide a reliable source of power for schools, hospitals, homes and businesses. Oliveira Energia and local Cat dealer, Sotreq, found a way. Together they completed a new power plant on time and on budget, and Cat equipment provides 107MW of power with 90+ percent availability.


Electric Power products

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products

PEAK SHAVING KEEPS ELECTRICITY RATES STEADY

PEAK SHAVING KEEPS ELECTRICITY RATES STEADY

Cat® gen sets help manage resources and keep the cost of power down. Onsite generation and local Cat dealer enabled Heber Light & Power to keep rates stable for 10 years. See how they do it.

View Customer Stories

Brochures

View our power generation brochures

Caterpillar offers standard and customized power solutions for all your applications, where you need it, whenever you need it.

View Brochures

White Paper

White Paper

Caterpillar is pleased to provide information on new technologies as well as innovative solutions to power your business.

View White Papers

Meeting Base or Peak Loads with Natural Gas

Electric utilities can operate gas engine generators continuously to serve base electrical loads. This is particularly advantageous in the absence of a reliable centralized power plant, or where the economics and availability of natural gas fuel are key drivers.

Gas engine generators are also commonly used to handle peak loads. Spikes in demand for utility grid electric power typically occur in the early morning before the workday, and in the late afternoon after the workday ends. Most people can relate to getting home from work and immediately flipping the light switch, turning up the heat or air conditioning and tuning in to the local news on television. When thousands of people collectively engage in the same behavior, large spikes in power consumption occur for a relatively short period of time. Some utilities choose to enter into long-term power purchase agreements to own a reserve block of power to address these intermittent spikes. However, this approach can lead to unnecessary base load capacity, driving up costs for the utility and its customers.

Caterpillar will give you expert consultation on how to design, install, and maintain power plants designed for utility applications.

Benefits from utility gas generator applications include:

  • Reduced energy costs
  • Efficient use of resources
  • Increased revenue opportunities

How It Works

Baseload generator power plants can range in size from just a few megawatts (MW) for a small island to over 100 MW for larger metropolitan areas. These power plants can be built with multiple 2 to 6 MW size class generators operating in parallel as a central source of electricity for the local electric grid.

Typical peaking power plant solutions operate in the 2 to 50 MW range from 100 to 3,000 hours per year. Most 100 hour-per-year plants would typically be diesel fueled and cover a super peak, while natural gas fueled power plant economics favor higher hour applications and longer duration peak demand.

Cat utility grade paralleling switchgear is used to operate multiple generators together and in parallel with the main utility grid. In open power markets, the power produced from these generators during the peak times of day can be dispatched to meet local customers' needs or sold in open, real-time markets at the spot price for a profit.

For emergency utility power shortages or outages, Caterpillar also provides utility scale gas rental power modules via Cat Rental Power that can be quickly dispatched and installed to make up immediate power shortages.

Cat® power stands up to Hurricane Sandy

When Hurricane Sandy made landfall, the Joint Meeting of Essex & Union Counties wastewater plant treated all the raw sewage that came into the facility during the storm. None of the treatment tanks overflowed, even when the nearby Elizabeth River and the Arthur Kill saltwater channel flowed in.

Learn More
Project Financing

No project is the same - from the application to the power need. That's why we offer a range of project financing options.

See our Offers
Precision Sizing at Your Fingertips.

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat® Electric Power SpecSizer.

Learn More
Electric Power Social Media

Check out the Cat® Electric Power social media page for the latest news, preventive maintenance tips, and product and show announcements.

Learn More
Cat® Dealer Service

The Cat dealer network is always ready to help. Find your dealer and read the latest in electric power service and support.

Get in touch today
Project Financing

No project is the same - from the application to the power need. That’s why we offer a range of project financing options.

See Our Offers
Electric Power News

Read the latest electric power news and articles relating to Cat electric power products by people in the know, on topics that matter to your business.

READ MORE