Caterpillar Introduces 50-Hz Cat® 3516E Diesel Generator Set Featuring Industry-Lowest Footprint and Weight at 3000 kVA Standby Rating

For Worldwide Release: May 24, 2016
Release Number: EEPR0416

PEORIA, IL – Caterpillar Inc. today announced the introduction of the Cat® 3516E diesel generator set with a 3,000 kVA standby rating in 50 Hz operating environments, which offers the lowest footprint and weight in this power range.

With a footprint of 15.84 square meters and weighing 20,048 kg, the Cat 3516E generator set requires up to 32 percent less installed space and is about 27 percent lighter than competitive offerings, translating into lower handling costs, reduced expenditures for foundations and supporting structures, and more space for business operations.

Available now, the Cat 3516E generator set is powered by the proven 3500 Series engine, the industry standard for large diesel engines.  This engine platform has offered reliable performance for 35 years, with hundreds of thousands of installations worldwide.

Featuring a 78.1-liter displacement, the 3516E engine utilizes the Cat A5 engine control module (ECM), which enables a fast response to load changes, minimizing power quality issues.  The A5 ECM also offers increased I/O capability for enhanced monitoring and control capabilities.

The Cat 3516E diesel generator set is available with either a standard 43oC ambient radiator or a 50oC high-ambient radiator, which delivers full power from the generator sets at ambient temperatures up to 50oC with no derating, supplying power when it is most needed.

The factory installed radiators were designed by Caterpillar specifically for the 3516E generator set package.  A four-point lift for the entire generator set includes the radiator with a complete coolant fill, allowing customers to position the generator set with very little local assembly.

An auto tensioner for the radiator fan belts reduces maintenance costs by eliminating the need for checking belt tension during service intervals.

Configured in low or high voltage applications, the Cat 3516E generator set features the motor starting capabilities needed for quick load acceptance.

Caterpillar is a leader in the power generation marketplace with power systems engineered to deliver unmatched durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service every aspect of Cat equipment.

For more information, visit www.cat.com/powergeneration or e-mail cat_power@cat.com. To interact with other power generation professionals in our online community, register at www.catelectricpowerinfo.com/connect.

Image Downloads

3516E Engine

 

 

# # #

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2015 sales and revenues of $47.01 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries and Power Systems - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow,” the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission. 

©2016 Caterpillar All Rights Reserved. 

Press Inquiries

Bob Chase 
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Rachel Perva
Caterpillar Inc.
Tel: +1 309-675-7267
perva_rachel@cat.com

Reader Requests Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610