Cat® Tilt Buckets Handle Angled -Surface and Precision- Grading Tasks

For Release in North America, Europe, Australia, New Zealand: September 2016
Release Number: 439PR16

A new line of Cat® tilt buckets is available for Cat crawler-excavator models 311-325 and for wheel excavator models M314–M322. The new buckets, available in both pin-on and coupler configurations, hydraulically tilt 45 degrees from vertical, right and left, to provide added capability when working on angled surfaces or performing precise grading. The buckets install easily and are designed for such applications as ditch cleaning, landscaping, and various construction tasks. In addition, the buckets can be used for conventional excavating in low-impact soils, including top soil and clay.

The tilt buckets are equipped with two horizontal cylinders—sized to provide forces matched to the machine—that allow the operator to position the bucket and maintain grade without moving the machine. The horizontal-cylinder design allows a low-profile for the bucket, while protecting the cylinders from material flow.

Grade-control ready

The new buckets are drilled and tapped to accept the bolt-on sensor and clips required to make them “plug-and-play” compatible with Cat Grade Control 3D. Grade control provides visual and audio positioning guidance for the operator via the machine’s in-cab monitor, enhancing the speed, accuracy, and material-movement efficiency of excavating and grading tasks.

Bucket protection

Tilt buckets feature a reversible, wear-resistant, bolt-on cutting edge that protects the base edge and provides extended service life. In addition, bucket surfaces subject to heavy wear, such as corners, are protected with replaceable, weld-in inserts of premium-grade steel (400 BHN).

Caterpillar supports its work tools with a comprehensive range of pre- and after-sales services, from advice about work-tool selection to operator training, equipment management, and financial and insurance products.

###

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission. 

©2016 Caterpillar All Rights Reserved

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests www.cat.com/requestCatinfo