GENERATORS FOR GREENHOUSE FACILITIES

GREENHOUSES

Greenhouses

Install generators that grow your business.

Greenhouses require energy to thrive — they require time and resources. We’re helping make your business better with power built to cut costs and boost plant health. Cat® combined heat and power (CHP) systems are engineered to produce electricity for your operation while heating your facility. Fueled by natural gas, our CHP generators for greenhouse facilities run at an efficiency of more than 90 percent. A Cat aftertreament system filters exhaust gas, rich in carbon dioxide, to be used as plant root fertilizer.

Even sell excess energy to your local grid with our utility grade paralleling switchgear and controls.

Whether it’s an estimate, installation or on-site service, we’re committed to ensuring you get quality from our systems and expert support from our Cat team.

Cat Generator Sets: How Combined Heat and Power (CHP) Works in Greenhouses

Combined heat and power systems provide a profitable and sustainable solution for greenhouses. By generating thermal energy and electrical energy simultaneously, a CHP system can yield a fuel efficiency rate over 90% versus the typical boiler efficiency of 40-50%. Typical payback on these systems is less than 3-4 years.


Electric Power products

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products

Customer Stories

Customer Stories

It takes a lot of energy to generate the necessary heat to grow flowers year-round. Rosa Flora, in Ontario Canada, accomplishes this with the aid of its own combined heat and power (CHP) system. They have always counted on their local Cat dealer to have whatever they need, whenever they need it.

View Customer Stories

Brochures

View our power generation brochures

Caterpillar offers standard and customized power solutions for all your applications, where you need it, whenever you need it.

View Brochures

White Paper

White Paper

Caterpillar is pleased to provide information on new technologies as well as innovative solutions to power your business.

View White Papers

High-Efficiency Power Systems

Greenhouse facilities reduce operating costs by implementing a Cat combined heat and power (CHP) system using clean pipeline natural gas as a fuel source. Cat gas generators for greenhouse facilities can provide electricity for electrical loads, heat energy for warming of the greenhouse, and recycled carbon dioxide from the engine exhaust as an organic fertilizer.

Benefits from greenhouse CHP projects include:

  • Energy efficiency over 90 percent
  • Reduced energy costs and emissions versus separate heat and electrical generation systems
  • Increased revenue opportunities through the export of electricity
  • Carbon dioxide crop fertilization

How It Works

Any Cat natural gas fueled engine can be configured specifically for applications involving heat recovery. The engine drives a Cat generator for greenhouse facilities to produce electricity, while jacket water and/or exhaust cooling circuits are fed through heat exchangers to transfer the waste heat from the engine to a hot water holding tank. That hot water is stored and used to keep the greenhouse warm. Oxidation catalysts can be used to remove carbon monoxide, and a urea based SCR system is employed to reduce NOx to just a few parts per million. The result is an exhaust gas so clean it is piped to the greenhouse plants' roots as a fertilizer, boosting farmers' yields.

Since sizing based on heat load is the key driver, the electricity produced at a greenhouse often exceeds the local demand. Many countries throughout Europe incentivize high-efficiency electric power generation via production credits and most electricity produced is exported to the local grid. In other parts of the world, grid unreliability and pure economics are driving greenhouse agriculture toward similar solutions.

Caterpillar provides customized CHP package proposals, including the required mechanical equipment and controls to capture and transfer the engine thermal energy to a greenhouse facility. In addition, Caterpillar offers the required exhaust emissions aftertreatment, utility grade paralleling switchgear, and controls to sell excess electricity generated to the local electric grid.

The total energy cost savings of such systems can more than offset the total owning and operating costs, delivering a payback in as little as two to three years, depending on local energy pricing and policies.

Bountiful Harvest

Harvest Power and Caterpillar are deploying a unique waste-to-energy solution in Orlando, Florida, turning food waste into power. The bountiful harvest process uses anaerobic digestion to produce renewable biogas, which powers two Cat® generator sets that produce 5.4 MW of combined heat and power—enough energy to power more than 2,000 homes each year.

Learn More
Power Systems Training

Your Cat® dealer is the best resource to help you meet your energy needs in terms of products, service, and skills acquisition. Work with your local Cat dealer to get the best training and support for the life of your products.

Learn More
Electric Power Application Centre

SpecSizer evaluates load types, collects data and organizes it to help you select the generator set that’s best for you. Find product comparisons, technical data, product sizing and more using our technical information portal (TIP) specifically created for consultants, architects, engineers, and owners. Check out these valuable resources now at our Application Centre!

Learn More
Electric Power Social Media

Check out the Cat® Electric Power social media page for the latest news, preventive maintenance tips, and product and show announcements.

Learn More
Cat® Dealer Service

The Cat dealer network is always ready to help. Find your dealer and read the latest in electric power service and support.

Get in touch today
Project Financing

No project is the same - from the application to the power need. That’s why we offer a range of project financing options.

See Our Offers
Electric Power News

Read the latest electric power news and articles relating to Cat electric power products by people in the know, on topics that matter to your business.

READ MORE