Cat® 336F/F L XE Hybrid Delivers Fuel-Efficient Production With Integrated Technology

For Release in Japan: September 2016
Release Number: 313PR16

The Cat® 336F/F L XE Hybrid features an integrated design that conserves fuel, optimizes performance, and captures and reuses energy. The machine delivers an estimated fuel savings of up to 13 percent compared with its standard 336 counterpart with no compromise in performance and no added maintenance costs. The new Cat Production Measurement system adds even more value by enabling operators to load trucks with just the right weight while allowing managers to remotely monitor the machine’s productivity.

The 234 kW (ISO14396) C9.3 ACERT™ engine meets Japan 2014 (Tier 4 Final) emissions standards without interrupting the operator or the job. Proven electronic, fuel, air, and aftertreatment components ensure customer expectations for productivity, fuel efficiency, reliability, and service life are met. The inherent fuel efficiency of the C9.3 ACERT engine is further enhanced with automatic engine speed control, a programmable engine idle shutdown feature, and an ECO mode that allows operators to tailor machine performance to the application.

The 336F/F L XE uses three building block technologies to deliver outstanding fuel savings and performance. The Cat Electronic Standardized Programmable (ESP) pump smoothly transitions between the hydraulic hybrid power sources, the engine, and the accumulator to conserve fuel. The Cat Adaptive Control System (ACS) valve optimizes performance by intelligently managing restrictions and flows to control machine motion. Instead of wasting kinetic energy during swing braking, the Cat Hydraulic Hybrid Swing System pressurizes the accumulator to stop the machine and then uses that pressure when needed to accelerate the machine later.

The key ingredient is the ACS valve, which can only be found on the Cat brand. It is the “brain” of the system – one that independently controls machine functions and directs hydraulic energy where operators need it precisely when they need it. Because the ACS valve is fully integrated with the pump and hybrid system, operators will experience the same extraordinary control and hydraulic power they get from traditional Cat machines with the added benefit of dramatically reduced fuel consumption. That’s why the valve is now standard on larger machines like the 374F L and 390F L. 

Technology enhancements

To assist customers in managing the 336F/F L XE for optimum return on investment, Caterpillar offers several connected technologies as standard.  Grade technologies provide real-time bucket tip elevation guidance to help operators stay on grade and finish work more quickly, accurately, and productively. The latest technology addition is payload, and it provides real-time weighing as the boom swings for fast, efficient loading, and optimum payloads. Operators can view load weights on the in-cab display and know when target payload is achieved, maximizing the productivity of the entire fleet. Productivity can be tracked from the cab—with quick access to payload weights, load and cycle counts, and daily totals. Site managers can wirelessly access payload data and machine operating data such as location, hours, idle time, fuel usage and events via Link technologies through the VisionLink® web portal to measure production, monitor efficiency, and optimize performance.

The 336F/F L XE's massive frame, heavy-duty extended-length undercarriage, and standard and heavy counterweight options combine to form an exceptionally strong, stable work platform for digging, lifting, or attachment use. The heavy-duty reach boom can be paired with either a 2.8 m or 3.2 m or a 3.9 m stick. A 6.18 m mass boom and 2.55 m stick combination are also available. So are multiple Cat Work Tools and a state-of-the-art tool control system designed specifically to help customers get the most out of one machine.

The 336F/F L XE also provides the ultimate in operator comfort and convenience, featuring a spacious operator's environment. Air suspension and heated and cooled seats are available as well as joystick controls adjustable to suit operator preferences and an automatic climate control system that continually maintains a comfortable environment.

Serviceability features include ground-level access to major maintenance points, electric fuel system priming pump, remote fuel tank drain, and a fuel level indicator to help avoid overfilling. Safety features include a Roll-Over Protective Structure (ROPS) cab, anti-skid surfaces, programmable halogen working lights, easily stored upper and lower windows, and large skylight that can be removed for an emergency exit.

For more information visit www.cat.com.

 

336F/F L XE HEX Product Specifications

   

Engine

Cat C9.3 ACERT

Net Power Rating (SAE J1349 / ISO9249)

306 hp (228 kW)

Operating Weight

336F XE: 35000kg

336F LXE: 36000kg

Max. Dig Depth *

7 390 mm

Max. Reach @ Ground Level *

10 920 mm

*with Reach boom 6.5m, R3.2DB stick, 1.5m3 bucket

# # #

Price

336F XE (Standard configuration):  37,762,000 yen (Tax not included)

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

 

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission. 

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2016 Caterpillar All Rights Reserved

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Product Page

Reader Requests

http://www.cat.com/en_US/products/new/equipment/excavators.html

www.cat.com/requestCatinfo