Valve Misfire Detected and Corrected Without Expensive Repair

 

What happened?
An unmanned natural gas compressor station based in the United States is equipped with four compressor packages and monitored remotely with Cat® Equipment Care Advisor (ECA). ECA analytics detected a misfire on two cylinders of a G3608 engine. At the time the misfire was discovered, it wasn’t impairing performance or causing engine damage.

What action was taken?
The Fleet Advisor recommended that the pre-chamber needle valve be temporarily adjusted, then returned to its normal position if minor clogging occurred in the valve. This procedure stopped the misfire. What is the value to the customer? The customer benefited in several ways:

  • No unnecessary parts replacement. The issue was corrected without replacing the parts (spark plugs and check valves). As a result, the customer didn’t lose the value remaining in the existing parts and didn’t have to spend approximately $1,250 for replacement parts and the labor to install them.
  • No lost revenue from an unnecessary shutdown. Because the situation was resolved without an inspection or repair, production wasn’t interrupted unnecessarily.
  • No unscheduled downtime. The proactive valve adjustment reduced the risk of a future failure that could have resulted in an unscheduled outage and lost production estimated at $1,500.

The total value derived from this single issue is approximately $2,750. The cost of the service is $400 per month at 98% run time.


Oil & Gas Customer Stories

Oil & Gas Customer Stories valve misfire detected and corrected

Oil & Gas Cat Connect

Oil & Gas Cat Connect

You need hard facts about your oil & gas equipment. Lots of them. About how well your assets are working. And how efficiently your operation is running. Fortunately, equipment management technology is built into today's equipment and can give you the timely information you need.

Learn More