Caterpillar Launches Cat® C15 and C18 China Phase IV Power Solutions at 2014 CIPPE in Beijing, China

For Worldwide Release: March 2014
Release Number: CO&G14PR5

Beijing, ChinaCaterpillar Oil & Gas is pleased to announce the production and availability of the new Cat® C15 ACERT™ engine and C18 engines. Designed for workover and mobile drilling rigs, the new Cat C15 and C18 engine deliver reliable horsepower while meeting the newly-enacted Phase IV emissions regulations in China. The Phase IV compliant Cat C15 engine with aftertreatment packaged with a Cat CX31 transmission will be on display at the Caterpillar booth at the 14th China International Petroleum and Petrochemical Technology and Equipment Exhibition (CIPPE) from March 19th to 21st in Beijing, China.

“We developed these engines to not only comply with the legislation impacting the China oil and gas market but to also offer our well services customers in the region reliable power in workover and drilling applications,” Scott Roberts, Caterpillar Oil & Gas well service product marketing manager said. “Both engines complement our existing offerings developed specifically for our Chinese customers and feature tailored custom packaging options to create a one-of-a kind solution.”

The Cat C15 ACERT On Highway China Phase IV engine features a power rating of 540 bhp (403 bkW) @ 1800-2100 rpm and the Cat C18 On Highway China Phase IV engine is available in a power rating of 630 bhp (470 bkW) @ 1800-1900 rpm. Both engines offer industry-leading power and torque capabilities optimized for drilling and workover applications. Emissions solutions for the Phase IV Cat C15 and C18 include an on-engine NOx Reduction System (NRS) and aftertreatment featuring a Clean Emissions Module.

The engines offer robust validation on 350ppm fuel sulfur.  Additionally the Cat C15 and C18 are offered with a variety of attachments to ensure ease of integration into application, with standard ADEM A4 engine management system and can be ordered with optional attachments including an engine-mounted transmission oil cooler, air shutoff valve, radiator etc. for drilling and workover rig applications.  The Cat C15 is optimized to be paired with the Cat CX31-P600 transmission.

“In addition to a low total cost of ownership, the Cat C15 and C18 offer a broad operating speed range and high power density, which are both critical for well service applications,” Roberts continued,“Additionally, customers can be confident in the unmatched service and coverage Cat dealers offer specifically in the China market.”

All Cat Oil & Gas products are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. To learn more about these or other Cat products, please visit the company’s booth at the 2014 CIPPE Beijing event, Hall W1, Booth W1503.  For more information, visit www.catoilandgasinfo.com/.

For up to the minute information on Caterpillar Oil & Gas, follow us on Facebook: http://www.facebook.com/caterpillaroilandgas & Twitter: http://www.twitter.com/catoilandgas.

# # #

About Caterpillar Oil & Gas
Caterpillar Oil & Gas, with headquarters in Houston, Texas, United States, groups all the sales and service activities for Cat oil and gas power solutions within Caterpillar Inc. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW.  The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: www.catoilandgasinfo.com

About Caterpillar
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

Press Inquiries
Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449
Marcoux_Jenna_J@cat.com