Caterpillar Ships First MaK™ Dual Fuel Engine

For Worldwide Release: July 2013

Release Number: M7PR13

Caterpillar Marine Power Systems is pleased to announce the shipment of the first MaK™ M 46 DF dual fuel marine engine. The M 46 DF, Caterpillar’s first marine dual fuel solution, will power a newbuild ordered by Germany’s AIDA cruises. Three 12 M 43 C marine engines will also power the cruise liner. The engine left the MaK Rostock, Germany facility en route to Mitsubishi Heavy Industries in Japan. Upon arrival, it will immediately be placed in the ship’s hull.

“We’re pleased to deliver our first dual fuel marine product to AIDA cruise lines, a longtime collaborator and partner” said Detlef Kirste, Caterpillar Marine Power Systems Senior Product Definition Engineer. “The M 46 DF will provide AIDA with superior performance and operational flexibility without sacrificing power or reliability.”

Able to alternate from gas to diesel mode during operation, the M 46 DF offers the flexibility to operate vessels reliably in all geographical areas, whether the fuel in use is gas, marine diesel oil (MDO) or heavy fuel oil (HFO). In gas mode, the M 46 DF features industry-leading fuel consumption and will comply with IMO III as well as EPA Tier 4 regulations. The engine has been designed to allow retrofitting of current M 43 C engines.

With a bore of 460 millimeters and stroke of 610, the engine was designed for electric drive propulsion systems as well as mechanical propulsion systems. Although designed for unlimited operation on LNG, marine diesel oil and heavy fuel oil, the M 46 DF will reach industry- leading efficiency in gas mode.

Caterpillar offers its renowned service and support for the MaK dual fuel engine, including installation and application, system integration support, as well as customer and crew training. The M 46 DF is distributed and sold through Caterpillar’s MaK dealer network.

For more information about Caterpillar and MaK marine engines, please visit MARINE.CAT.COM/pr

# # #

About Caterpillar Marine Power Systems

Caterpillar Marine Power Systems, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat® and MaK marine engines within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100  kWe in marine generator sets. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: MARINE.CAT.COM/pr

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

Press Inquiries

Caterpillar Marine Power Systems Communications
Jenna Janik:

Reader Requests