Caterpillar to Showcase Cat® C32 EPA Tier 3 Marine Propulsion Engine, Expanded Offerings at 2013 International Workboat Show

For Worldwide Release: October 2013
Release Number: M14PR13

Caterpillar Marine Power Systems will highlight its wide array of U.S. EPA Tier 3/IMO II certified marine power solutions at the upcoming International Workboat Show held October 9th – 11th in New Orleans, Louisiana. On display at the Caterpillar booth this year will be the Cat® C32 ACERT™ EPA Tier 3 certified marine engine, which is now also offered as an EPA Tier 3 certified auxiliary engine and an EPA Tier 3 certified generator set. Cat C32 marine power solutions are ideal for the tug and salvage industry, ferry and offshore applications, specifically crew boats, platform supply vessels and offshore supply vessels.

The C32 ACERT marine propulsion engine is available at ratings that meet both EPA Tier 3 and IMO II emissions regulations, while still offering seven Wide Operating Speed Range (WOSR) ratings. The C32 now has a separate circuit aftercooling system (SCAC) for three power ratings, ‘A’ through ‘C.’ The SCAC system is a significant benefit for customers as the system removes seawater from the coolers, resulting in longer service intervals. Additionally several design changes have been engineered into the platform to lower operation costs, including longer oil change intervals. Customers will also be able to select from an increased amount of attachments and options when ordering the C32 ACERT Tier 3 engine, including a class-approvable alarm and protection system.

Other benefits include the proven engine’s extensive operating history and performance iron with thousands of validation testing hours for quality and durability. The C32 ACERT marine engine is backed by the stellar product service and support of the extensive Cat global dealer network as well as Caterpillar’s standard 12 month warranty. Extended Service Coverage is available on the C32 engine for up to 60 months or a maximum of 12,000 hours, depending on which criteria is met first.

“We’ve been very pleased with the success of the C32 in the field. We have accumulated over 50,000 hours of field testing to date, specifically in workboat applications.” Chad McIntosh, Caterpillar product definition manager said. “Built on the proven performance of the trusted C32 platform, the new C32 offering provides customers with design enhancements as well as the flexibility to operate in regulated waters with a Tier 3 certified power plant.”

Also available as of spring 2013 are the C32 auxiliary engine and generator set, both of which are EPA Tier 3 compliant. The auxiliary engine and generator set feature the same benefits and design enhancements offered on the C32 marine engine platform. The C32 generator set is also available in new voltage offerings and performs with an increased electrical power output of 3% on average.

For more information on the Cat C32 EPA Tier marine power solutions, please visit the Caterpillar booth #2802 and #2902 at the International Workboat Show, in New Orleans, Louisiana on October 9-11th . For up to the minute updates at the show, please follow us on Twitter: and Facebook: using #catatwbs. Unable to make the show? Learn more about comprehensive Cat offerings at

# # #

About Caterpillar Marine Power Systems
Caterpillar Marine Power Systems, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine engines within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are. More information is available at: MARINE.CAT.COM/pr

About Caterpillar
For more than 85 years, Caterpillar Inc. has been making progress possible and driving positive and sustainable change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is a technology leader and the world’s leading manufacturer of construction and mining equipment, clean diesel and natural gas engines and industrial gas turbines. More information is available at

Press Inquiries
Jenna Janik Marcoux
Phone: +1 713 895 1449