RESEARCHERS RECEIVE FUNDING TO TURN WASTE INTO POWER SOURCE FOR SPACE MISSIONS

Researchers receive funding to turn waste into power source for space missions


The South Dakota School of Mines & Technology has been awarded $750,000 to develop an extreme biological system to turn solid waste into a power source to create an efficient alternative to the current processes using chemical fuel cells, such as hydrogen fuel cells, that require pure chemicals.

South Dakota School of Mines & Technology
07/07/2016

The South Dakota School of Mines & Technology has been awarded $750,000 to develop an extreme biological system to turn solid waste into a power source for long-term space missions.

The NASA EPSCoR award builds upon earlier waste conversion concepts developed through Venkataramana Gadhamshetty's research. Earlier this year, Gadhamshetty, Ph.D., P.E., BCEE., and his research team announced it had converted discarded tomatoes into electricity. 

There is a critical need for a similar product for NASA, where long-term, manned space missions are challenged by waste-treatment and power requirements. During space missions, each crew member typically generates 3.6 pounds of solid waste from biodegradable (such as food) and non-biodegradable (such as plastic) sources daily. 

This voluminous waste is a burden to space missions, as it increases fuel consumption and may create nuisance and health concerns due to the pathogens. The South Dakota Mines approach will use unique microorganisms isolated from the deep levels of the Sanford Underground Research Facility (SURF) in lead as test subjects to develop an advanced biological module that uses electrochemistry principles, operates at thermophilic conditions and generates electric power from solid wastes in a single step.

The project will result in an efficient alternative to the current processes using chemical fuel cells, such as hydrogen fuel cells that require pure chemicals.

"These SURF extremophiles are known to survive harsh environments typical to extraterrestrial space, where it is seemingly uninhabitable. The extremophile biology provides a platform for provocative research to develop bio-modules to generate electricity from solid form of wastes, inhibit pathogens in human waste, and recycle the waste during space missions," said Gadhamshetty, of the department of civil & environmental engineering.

A group led by Rajesh Sani, Ph.D., from SD Mines' Department of Chemical & Biological Engineering, have isolated the SURF extremophiles.

"Using organisms that adapted to survive in one of the more extreme environments on earth to advance science for space travel is a novel concept. I'm glad NASA is interested and willing to support this work," said SD Mines president Heather Wilson.

Researchers will collaborate with experts at Argonne National Laboratory and Navy Research Laboratory and throughout industry to develop a stacked bioelectrochemical module that supports low-powered electronics, including a Mars microrover. Resources from NASA's Jet Propulsion Laboratory, Kennedy Space Center and Ames Research Center will also be used.

The project addresses three prime focal areas identified for research and economic development in South Dakota—energy and environment, value-added agriculture and agribusiness, and materials and advanced manufacturing.

The program will provide support for seven PhD students and offer opportunities for research collaborations with the University of South Dakota, South Dakota State University and two tribal colleges, as well as six industrial partners.

"This multidisciplinary NASA project has become a reality only due to the exceptional range of interdisciplinary researchers—catalysis, extremophile biology, environmental and chemical engineering, and nanotechnology—from South Dakota Mines, South Dakota State University, University of South Dakota, and several businesses, including Hexpoint technologies," Gadhamshetty said. The research team originally received a Research Initiation Grant from SD NASA EPSCoR in 2015 to develop the collaborations within South Dakota and with NASA researchers and to obtain preliminary results.

South Dakota School of Mines & Technology

www.sdsmt.edu 

- Edited by Chris Vavra, production editor, Control Engineering, CFE Media, cvavra@cfemedia.com. See more Control Engineering energy and power stories.

 


Waste gas into power

Cat gen sets now run a renewable energy power plant to generate electrical power by capturing and conditioning the landfill gas.

The F.R. Bowerman Landfill contains an estimated 31 million tons of waste, producing methane gas. In order to better manage and reuse this onsite waste, Cat® gen sets now run a renewable energy power plant to generate electrical power by capturing and conditioning the landfill gas.

READ THE STORY

Innovation
This is the Age of Smart Iron.

Caterpillar has spent over ninety years committed to innovation and technology

Caterpillar has spent over ninety years committed to innovation and technology that help our customers succeed. Advancements come faster than ever before and where connectivity drives productivity as your industry evolves.

LEARN MORE

Cost-efficient continuous power generation

Two biogas-fueled Cat gen sets at Nong Rai Farm produce nearly 200 kW

Two biogas-fueled Cat gen sets at Nong Rai Farm produce nearly 200 kW. The power plant meets all the farm’s power needs and saves 2.8 million baht annually that would have been spent purchasing electricity from the local power grid.

SEE THE WHOLE STORY