Attendees Remotely Operate Cat® Machines at CONEXPO

CONEXPO , CON/AGG

State of Washington road maintenance crews have dealt with a winter full of danger, clearing snowy roads and doing avalanche control work. Safety is a year-round concern for Department of Transportation workers.  So at CONEXPO-CON/AGG 2017, Mike Brace, who supervises road maintenance crews for Washington State DOT, got a first-hand look at how the state-of-the-art remote technology of Cat® COMMAND can keep workers safe.

From a comfortable remote operator station in Las Vegas, Brace ran by remote control a Cat® D8T, located 1,400 miles away in Peoria, Illinois.  “You can see it on the screen what I’m actually doing and how it’s moving,” says Brace. “It’s such a pleasure to run, too. It’s effortless.”

 

“YOU CAN SEE IT ON THE SCREEN WHAT I’M ACTUALLY DOING AND HOW IT’S MOVING. IT’S SUCH A PLEASURE TO RUN, TOO. IT’S EFFORTLESS.”

 

Cat® COMMAND allows the operator to stay out of harm’s way, using either an over-the-shoulder operator console or a remote operator station offering line-of-sight and non-line-of-sight control.  “The controls are fully integrated into the machines’ systems for quick response and smooth operation,” according to Alan Pumklin, one of the Caterpillar technology experts at CONEXPO.

Operators of smaller Cat machines can also work safely outside the cab with RemoteTask™. Operators can use the remote control system with wireless control up to 1000 feet line-of-sight, while giving up nothing in efficiency and accuracy. “You can position yourself in a location where you can see what you’re doing to make a decision before you make the next move,” says Caterpillar Technology Expert Dante Thomas.

See the Cat® COMMAND and RemoteTask™ technologies for yourself at CONEXPO-CON/AGG in Las Vegas March 7-11.  Visit the D8T Remote Operation Station in the Gold Lot and run a D8 in Peoria live from Las Vegas. Also in the Gold Lot, see the 988K Display with Cat COMMAND for loading.  And at five minutes past every hour, experience the Cat 259D Compact Track Loader with RemoteTask™ demonstration in the Gold Lot.

 

Attendees try out Cat® COMMAND and RemoteTask™ remote control systems at CONEXPO-CON/AGG 2017.

Safety And Efficiency Are Automatic With Cat® COMMAND, RemoteTask™


Operators can safely operate Cat® machines from outside the cab with Cat COMMAND and RemoteTask™ remote control system.

Read More

Cat® COMMAND


COMMAND enables you to implement remote control, semi-autonomous or fully autonomous mining equipment systems - offering unprecedented improvements in operator safety, equipment availability and site productivity.

Learn More

RemoteTask™

Designed for all Cat® D Series loaders, RemoteTask™ was created for one purpose: to remove the operator from the cab without sacrificing anything in terms of operational control, feel, and accuracy.

Visit RemoteTask Website
Construction Material Company Relies On Cat 986K, Cat Technology

Construction company Edward C. Levy relies on new Cat® 986K for superior performance, lowest operator cost.

Learn More
Technology Provides Edge

With 600 Cat machines in its fleet, Minnesota-based Veit & Company relies on the latest equipment technology to keep outworking the competition.

Learn More
NASCAR Driver Operates D11T from Miles Away

Ryan Newman, who races the No. 31 Caterpillar Chevrolet in the Sprint Cup Series, remotely operated a D11T Dozer from a trailer at the Phoenix International Raceway on November 13.

Learn More