U.S. Recycler Boosts Daily Productivity Using New Cat® Scrap Shear

When you process more than 40,000 net tons of recycled material a year, you need equipment that helps you get the job done as quickly and productively as possible. That’s why Rivers Edge Scrap Management relies on a range of Cat® machines and work tools.

The Kansas City-based company—which specializes in processing and recycling ferrous and non-ferrous scrap, along with e-waste such as cell phones, computers and batteries—recently mounted a Cat S3070 scrap shear on its 336FL hydraulic excavator.

Designed specifically for excavators working in scrap and demolition applications, the S3070 offers an ideal force-to-weight ratio that yields faster cycle times and more cuts per hour. Its 360-degree rotating configuration allows the shear to be positioned in optimum cutting positions without moving the carrier.

 

Both features help speed processing work, a benefit Rivers Edge has experienced firsthand.

“The performance of the scrap shear, as well as the perfect match between the work tool and machine, allows us to maximize our productivity,” says Tim Kates, Rivers Edge vice president. “We’ve compared the Cat S3070 shear and its equivalent from the competition. Its robustness, speed and performance is superior, which is increasing our daily productivity. It’s also easier to handle and it has more visibility—this has a major impact on safety on the site.”

 

“THE PERFORMANCE OF THE SCRAP SHEAR, AS WELL AS THE PERFECT MATCH BETWEEN THE WORK TOOL AND MACHINE, ALLOWS US TO MAXIMIZE OUR PRODUCTIVITY.”

 

But productivity and performance aren’t the only reasons Rivers Edge chooses Cat products. Kates points to Cat dealer service and the resulting good resale value as other important factors in the company’s purchasing decisions.

“We rely on the quality of Cat machines and work tools, as well as the service provided by Foley Equipment,” he says.

 

SEE THIS SCRAP SHEAR AT CONEXPO-CON/AGG 2017 – LEARN MORE

 

RELATED STORIES:


6 Tips for Boosting Productivity with Attachments


How do you choose the work tools that create the optimal pairing with your machine? These six suggestions will help you achieve the best productivity for your money.

Get Tips

S3070 Scrap Shear

Designed to fit 29- to 90-ton excavators, the S3070 rotating shear cuts when and how you need, with full bi-directional rotation for total control.

Learn More
Pacific Steel & Recycling Relies on Fleet of Cat® Equipment

Employee-owned Pacific Steel & Recycling, with nearly four-dozen scrapyards across the U.S. Northwest, relies on its extensive fleet of Cat® equipment to help it increase inventory turns and lower processing costs.

Learn More
When It Comes to Reducing Cycle Times, Cat® Material Handlers Are a “Perfect Fit”

Enter the Cat® 385C Material Handler. Using this specially designed scrap and material handling machine, Nugent reduced its cycle times down to 15-17 seconds—a critical savings for an operation that unloads approximately 1,800 tons of material per hour.

Learn More
From a 747 to Scrap in Just Four Days Using Cat® Excavators

Old airplanes are no match for Brandon Arnold's two Cat® 345C L Excavators. His team can scrap a plane and have the parts ready for shipment and recycling in just a few days.

Learn More
Cat® Excavators Serve as the “Swiss Army Knife” of Machines for Demolition Company

One machine doing the work of many—that’s how demolition company Adamo Group uses its fleet of Cat® Excavators to take down buildings with surgical precision and speed.

Learn More