Power Profile - Chiron Life Sciences Center

Customer: Chiron Life Sciences Center

Location: Emeryville, California

Customer Buisness Issue: Reliable and uninterrupted power supply for pharmaceutical production facilities

Solution: Initial installation: One Cat® Uninterruptible Power Supply (UPS) 250 kVA
Secondary installation: One Cat 750kW generator set Cat UPS 330 kVA One ATS

Cat Dealer: Peterson Power Systems
San Leandro, California

Power Need

Manufacturing drugs to fight cancer and infectious diseases is a precise business that requires a reliable, continuous power source, which means the Chiron Corporation takes its power needs very seriously. The Emeryville, California-headquartered pharmaceutical company’s production facilities are regulated by the FDA and must adhere to specific rules in sterile fill areas. Several of these restrictions involve water circulation and clean airflow. “A minor power glitch, even one as short as a fraction of a second, stops the pumps that circulate the water,” said Hellmuth Zieleniewicz, Chiron Life Sciences Center project manager. If the pumps stop, water pressure is lost and atmospheric air is sucked into the system through open user valves, contaminating the system and resulting in hours of lost production time.

Solution

This is why the company relies on a Cat® UPS continuous power system. Chiron first purchased a Cat UPS 250 kVA backed up by a Cat generator set to protect production loads. Zieleniewicz was so pleased with its performance, he installed a Cat UPS 300 kVA integrated with a Cat 750 kW generator set and a Cat automatic transfer switch to protect the second production facility.

Result

The Cat UPS 300 kVA alone proved its worth in the first few months after installation in the fermentation/purification building by protecting critical loads during four separate power events. “With our Cat continuous power system, the power in our production facilities is well provided for,” said Zieleniewicz.


Electric Power products

power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products

PRECISION SIZING AT YOUR FINGERTIPS.

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat® Electric Power SpecSizer.

Learn More