Delivering Power to Support Hurricane Matthew Emergency Response

Hurricane Matthew

Caterpillar Defense & Federal Products Delivers 22 Mobile Generator Sets for Hurricane Matthew Emergency Response

As Hurricane Matthew was about to make landfall in the U.S., Caterpillar’s Defense & Federal Products (D&FP) division was mobilizing 22 mobile generator sets for use in the emergency response efforts.

On the morning of October 6, the U.S. federal government sent out a request for quote (as Hurricane Matthew approached the Bahamas) and by 6:30 that evening, Caterpillar was awarded the contract and mobilization began. When Matthew changed course the following day, the destination was changed to Cat® Dealer Yancey Cat and the XQ1000 and XQ800 units were delivered to their Austel, Georgia location.

John Holland, a New Jersey-based rental power manager for Cat Dealer Foley Inc., began soliciting dealer inventory to establish the closest resources to meet the quick delivery requirement.

Holland organized the 22 generator sets, and all necessary cables and hardware for operations. The mobilization required 22 semi-tractors with 44 drivers to comply with DOT driver on-duty limitations. Holland dispatched a Foley service technician to Austel with 22 Product Link™ PL 131 (GPS) tracking devices for installation once the units arrived.

 

 

The hurricane weakened, so the generator assets were not used. The units ultimately returned to their respective Cat dealers (Ohio Cat, H.O. Penn and Foley).

“Even though the generator sets were not needed, it was still a useful exercise,” Holland says. “It demonstrated that we can respond on short notice. We got the equipment there and met the timelines—everything was delivered and ready to roll.”

D&FP Provides Generator Support to FEMA

In an emergency, Caterpillar D&FP is prepared to deliver mobile power when and where it’s needed to the Federal Emergency Management Agency (FEMA).

On March 4, 2016, D&FP was selected to be one of five contractors awarded a $45 million, five-year indefinite delivery indefinite quantity contract from the Defense Logistics Agency (DLA) to provide generator support to FEMA. 

 

“EVEN THOUGH THE GENERATOR SETS WERE NOT NEEDED, IT WAS STILL A USEFUL EXERCISE. IT DEMONSTRATED THAT WE CAN RESPOND ON SHORT NOTICE. WE GOT THE EQUIPMENT THERE AND MET THE TIMELINES—EVERYTHING WAS DELIVERED AND READY TO ROLL.”

 

This contract provides for the rapid deployment of generator sets to support FEMA disaster relief operations in order to protect against, respond to, recover from, or mitigate against threatened or actual major or catastrophic disasters and emergencies – both natural and man-made, including acts of terror.

D&FP is the prime contractor for this contract, and Cat Dealer Foley is the key subcontractor. Foley Cat has a long history of supporting natural disaster relief efforts, including Hurricane Sandy, Hurricane Irene, 9/11 and many others.

Foley Cat works with multiple Cat dealers to secure the needed generator sets for each task order, including arranging for round trip shipping, bill of material coordination, dealer-to-dealer communications and rebilling, GPS tracking, task order tracking, 24/7 repair request and other items for Caterpillar.

As part of this contract, D&FP participated in a live FEMA exercise in July to demonstrate its readiness skills for seven generator set model sizes, ranging from 25 - 500 kW. These units were delivered by Cat Dealer Yancey to a FEMA distribution location in Atlanta, Georgia.

 

GET THE LATEST STORIES AND TIPS FROM CATERPILLAR – SIGN UP FOR OUR E-NEWSLETTER

 

RELATED STORIES:


Caterpillar Defense & Federal Products

Caterpillar Defense & Federal Products

Whether it's standard products, modification of existing products, or entirely new products, Caterpillar Defense & Federal Products is committed to all branches of the military and to U.S. federal civilian agencies.

Learn More

Engine Applications for Federal Agencies

Engine Applications for Federal Agencies

Cat® engines provide prime power to remote installations worldwide, propulsion for military vessels as well as engine power for tactical and support vehicles. They’re built to meet or exceed today's toughest standards.

Learn More
Eye of the Storm

Cat Rental Power network provides strong, coordinated response to customers affected by Hurricane Matthew. The storm caused damages estimated in excess of $10.5 billion.

Learn More
Efficient, Sustainable Power

The University of Maryland Upper Chesapeake Medical Center (UM UCMC) installed a new Cat® G3516H natural gas-fired generator set for 2 MW of sustainable power as part of a cost-effective combined heat and power (CHP) system to ensure continuous patient care.

Learn More
Cost-Effective Power

Heber Light & Power keeps the electricity flowing through a peak load shaving effort that includes nine gas generator sets from Caterpillar. Around the clock, analysts at Heber Light & Power examine hour-by-hour wholesale energy prices to determine the most cost-effective combination of potential power sources to meet demand at any given time.

Learn More
Powering Through Disaster

When Sandy’s storm surge reached New York City, it flooded streets, tunnels and subway lines and caused massive power outages throughout the city. When devastation like this occurs, quick response is essential to Caterpillar customers. Through the mobilization of temporary power to customers throughout the region, the Electric Power team and the Cat® dealer network supported the disaster recovery efforts.

Learn More