Road Maintenance Operators Give Cat® Stable Blade Their Highest Grade

Stable Blade

Troy Schroeder is blunt about what used to frustrate him on the job. “Life before Stable Blade was a headache.”  Schroeder is a motor grader operator for the McPherson County, Kansas Public Works Department.  He says road maintenance work inevitably meant rework as soon as something on the road would cause his machine to bounce. “You’ve got damage behind you on the road. You’ve got washboards. You’ve got wasted material. You’ve got more work that you have to backup and fix,” says Schroeder.

You can find Stable Blade technology only on Cat® motor graders. It’s a first-of-its kind, anti-balance system specifically designed for a motor grader and patented by Caterpillar. “Stable Blade is the biggest technological breakthrough since Caterpillar put joystick controls on a motor grader,” says Caterpillar Motor Grader Expert Wade Porter.

Stable Blade uses an on-board sensor to detect when a bounce is about to happen. Once the sensor detects the bounce, the machine speed is automatically controlled. “There’s no operator intervention required,” says Porter. “The operator can simply sit back, relax and worry about moving material. Stable Blade works in conjunction with the standard electronic throttle control feature that comes on every Cat motor grader.”

 

Listen to customers who have put the newly patented, first-of-its-kind, Cat® Motor Grader anti-bounce Stable Blade feature to work and realized the benefits of this breakthrough technology.

 

Luke Wanninger, an operator from Sumner County, Kansas, says Stable Blade has improved the quality of his ride and his roads. “You set your cruise, you go down the road and if (Stable Blade) senses any sort of bumps or anything, it’ll slow you down,” says Wanninger. “It’s the best feature I’ve noticed in Cat graders right now.”

David Reeves of Franklin County, Kansas also sees how Stable Blade eliminates the need for costly rework.  “You don’t get any of that washboard effect out of it,” says Reeves. “You’re not going forward and backward cleaning it up.”

With that kind of improved productivity and fuel burn savings of up to 14%, Troy Schroeder says Stable Blade is saving money for taxpayers.  “If you look at the amount of work done compared to fuel burned, you’re way ahead - no doubt about it.”

Stable Blade is the better way to run a motor grader.  And there’s no doubt about that.

 

GET THE LATEST STORIES AND TIPS FROM CATERPILLAR – SIGN UP FOR OUR E-NEWSLETTER

 

RELATED STORIES:


5 Reasons to Banish Motor Grader Bounce

5 Reasons to Banish Motor Grader Bounce

Controlling machine bounce is an everyday battle for motor grader operators. Find out the five reasons motor grader bounce threatens your bottom line.

Read More

14M3 Motor Grader

14M3 Motor Grader

The 14M3 features a host of integrated technology solutions that increase operator efficiency, boost productivity levels and lower owning and operating costs.

View Model
Retrofitted Motor Grader with 24,000 Hours Featured at CONEXPO

Retrofitted Cat® 160M Motor Grader takes center stage at CONEXPO -CON/AGG 2017 after running 24,000 hours on the same engine.

Learn More
Cat® Motor Graders Reach New Heights in Snow Removal

A Cat® M Series Motor Grader was put to the test last season as part of a team of machines that moves in to open the pass along the Continental Divide in the spring. Independence Pass has an annual average snowfall of more than 28 feet, so it’s very tough going in wet, heavy spring snow conditions.

Learn More
Customers Use Virtual Reality to Evaluate Motor Grader Cab Designs

The advantage of working in the virtual reality environment is that you can switch back and forth so customers can see the concepts side by side and instantly compare the key features.

Learn More