Road Construction Production Study

Traditional vs Technology Road Construction Comparison Study

 

You’ve probably heard the countless reasons machine technologies can help save you time and money. Recently, Caterpillar put these to the ultimate test by building two roads side by side in a first-of-its-kind production study. One road used traditional road construction processes while the other used the latest in technology. The results speak for themselves:

The Setup

Two roads, each 400 feet in length, were constructed at our Peoria Proving Grounds in Peoria, Illinois. The first was built using traditional processes. The second was built with Cat® Connect Technology & Services including telematics, machine control and guidance, payload, and intelligent compaction technologies.

The test was built to replicate an authentic worksite – a variety of machines, some Cat and some non Cat, were used. They included dozers, motor graders, soil compactors, articulated trucks, wheel loaders, pavers, dual drum vibratory compactors and on-highway trucks.

In the study, labor, material, equipment, and fuel utilization were quantified and used to calculate total costs and project hours for both roads. The cost savings using technology were then applied using an increment of one mile to determine the return on investment and subsequent profitability.

 

The Results

The technology constructed road resulted in:

  • 31% fewer man hours
  • 34% fewer equipment hours
  • 46% fewer project hours
  • 37% less fuel consumption
  • And an environmental benefit of saving 12 acres of forest

How far down the road do you have to go until you reach profitability?

The investment in technology on this new road is about $250,000.

On a road construction project of about 3 miles in length, it takes 79 working days with technology vs the 147 working days with traditional methods. But it’s still short of a return on investment. However, four miles is nearly the break-even point. That means for every mile thereafter, the customer is banking the profits.

 

CUSTOMERS REPORT THE ROAD TO PAYBACK, USING CAT CONNECT TECHNOLOGY, TAKES 6 MONTHS TO 1 YEAR.

 

Customers report the road to payback, using Cat Connect Technology, takes 6 months to 1 year. This investment puts them in the fast lane to less cost, increased quality and safety and on to the next project in record time.

Watch the video to see the full results.

 

Click here to download the full jobsite study report.

 

 

Related Stories


Cat® Connect Technology

This revolutionary Caterpillar solution is robust and factory integrated, and features a suite of Grade, Payload and Compact technology solutions.

Learn More

Building a Highway Means Building a Country

Over the past 20 years, Bosnia-Herzegovina has suffered through a horrendous war and the worldwide economic crisis. But the people of this area are resolute and not ones to give up easily – even after harsh ordeals. Today, the country and its people are on the rebound.

Read More
Cat® Technology Helps Excavating Contractor Move Forward

Cat® machines and technology help Boyce Excavating’s bottom line, especially AccuGrade™ Grade Control system, which allows crews to work approximately twice as fast. It’s what company President Jack Boyce sees as the biggest improvement in equipment he’s seen in his career.

Learn More
Game-Changing Technology Delivers Confidence And Cost Savings

MDP is a machine-integrated soil compaction measurement technology that evaluates rolling resistance. That resistance provides an indication of soil stiffness and load-bearing strength—and whether compaction is adequate to hold the road, parking lot, building or whatever is planned for a site.

Learn More
Excavating Company Doubles Sales with the Help Of Cat Connect Grade Technology

In December 2011, Don Nusbaum and Scott Duso, owners of D/N Excavating Inc., landed their first big job—site development for a new rental condominium project that included all utilities and roadwork. The timeframe was tight, just 10 months, and the two men faced a dilemma.

Learn More