Caterpillar Selected by Alliance Offshore to Power First Zentech R-550D Jackup Rig


Beijing, China - Caterpillar Oil & Gas announced today that the Cat® C175 and Cat 3512 generator sets have been selected to power the first Zentech R550-D jackup newbuild for Alliance Offshore in China. Five Cat C175 generator sets, each with rated power of 1833 ekW at 1200 rpm, will be used as the prime power for the jackup with 1x Cat 3512 generator set providing emergency power. The newbuild is currently being constructed by CSSC Huangpu Wenchong Shipbuilding Company in China and the Cat power solutions will be delivered in summer 2014. Cat dealer China Engineers Limited (CEL) led Caterpillar’s efforts on the project.

“We’re pleased to be selected to provide both main and emergency power for first R550D jackup rig ever constructed,” Tim Tian, Caterpillar Oil & Gas Asia Pacific China sales manager noted. “The Cat C175 is the industry leader for jackup rigs in the offshore industry, reliably powering jackup rigs operating around the globe drilling at varied depths.”

The Cat C175 is ideal for customers seeking a high power density and lower emissions offshore drilling module. Offering 20 percent more installed power than previous models, the C175-16 allows for deeper drilling and higher mud pump loading. Its compact footprint offers significant weight savings when compared to medium speed engines and allows for retrofit with today’s Cat 3516 module design.  In addition, its full featured control system provides for easy interface with the local rig network, and can be controlled and monitored remotely.

The C175-16 is also highly fuel efficient, incorporating a fuel system that uses a high pressure fuel pump and control valve that deliver multiple precise injections within a single combustion event. This results in lower emissions, improved performance and reduced fuel consumption. Driven by the ADEM™ A4 controller, the C175-16 engine management system features full redundancy and provides superior performance, even in the most demanding environments. The fuel system directly impacts customers overall owning and operating costs as the fuel consumption has been optimized for typical drilling load.

Caterpillar offshore experts will be on hand and available for questions at the Caterpillar #3341 at OTC Houston, May 5-9th. For up to the minute information during OTC, follow us on Facebook: & Twitter: using #OTCHOUSTON and #CatatOTC. For more information on the solutions and services Caterpillar Oil & Gas offers, please visit

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions that include reciprocating engines, generator sets, transmissions and well stimulation pumps. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations worldwide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at:


About Caterpillar

For more than 85 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company also is a leading services provider through Caterpillar Financial Services, Caterpillar Remanufacturing Services and Progress Rail Services. More information is available at:

More information is available at

Image 1

Press Inquiries
Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449