First Cat® 3500 Dual Fuel Generator Sets to Power Fast Ferries at 2016 Rio Olympics

Lafayette, IN - Caterpillar Marine and Cat® Dealer Pon Power are pleased to announce the first Cat 3512C marine generator sets with Dynamic Gas Blending™ (DGB™) have been selected to power Assessoria Transporte Aquaviaro fast ferries for the 2016 Olympics in Rio de Janeiro, Brazil. A total of 28 Cat generator sets will be installed on 7 aluminum-hull fast ferries, with 14x Cat 3512 generator sets and 14x Cat 9 generator sets providing prime and auxiliary power. Each 3512 generator set will provide 1550 eKW @ 60 Hz of rated power. One ferry will be equipped with the new Cat marine dual fuel solution and powered by compressed natural gas (CNG). The remaining six ferries are being constructed with the option to readily retrofit the engine room to include the Dynamic Gas Blending kits in the future.

“We’re pleased to unveil our first Cat Marine 3500 dual fuel solutions with Dynamic Gas Blending for such a significant global event,” Chris Chenette, Caterpillar Marine product value manager noted. “Assessoria Transporte Aquaviaro will be not only be able to optimize the efficiency of their vessels powered by Cat dual fuel solutions but also operate on the waters with the confidence and product support you can only get from Caterpillar.”

Cat dealer Pon Power led the Caterpillar efforts on the project and will continue to provide support, packaging and commissioning for the Cat power solutions. “We, as Pon Power, see gas as the future fuel for marine. We are happy to materialize the customer needs of Coco Yachts together with Caterpillar Marine,” said Thomas de Haas, Pon Power Director Marketing and New Business Development.

The ferries are being designed by Coco Yachts Holland B.V. of The Netherlands and built by Afai Southern Shipyards in China. CoCo Yachts is a Dutch design company specializing in the design of Aluminium catamarans, ranging from 5-85 meters. Each ferry will feature diesel electric propulsion (DEP) with azimuth thrusters and identical engine rooms. The Cat power solutions for the project will ship to the shipyard in December 2014.

Manufactured in Lafayette, Indiana, the Cat 3512 DGB generator set features a low pressure gas system with an approximately 70% maximum gas substitution rate across a wide load range. The IMO II-compliant generator set operates with diesel-like rated power and transient response while maintaining an overhaul life similar to a diesel engine. Operators can achieve significant fuel savings due to the stellar load factor and substitution rate. Ideal for high speed applications, the new Cat marine dual fuel solution is based on the highly successful Cat dual fuel application for land drilling which was introduced to the market in 2012. The Cat 3512 generator sets at 1550 eKW with Dynamic Gas Blending are available to order now from the Cat dealer network.

“The new Cat Marine dual fuel solution leverages the proven durability of the 3500 diesel engine while offering customers enhanced fuel flexibility and power redundancy to run diesel or gas,” Jason Spear, Caterpillar Marine product definition engineer noted. “Furthermore the DGB technology is integrated into the diesel injection system to ensure combustion is optimized as a factory-supported solution.”

# # #

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas engines as well propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100  kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: MARINE.CAT.COM/pr

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

 

Press Inquiries
Jenna Janik Marcoux
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com

Pon Power
Peter Snijders
Phone: +31 78 6420 420
Peter.snijders@pon-cat.com