Caterpillar Introduces Fifth Mobile Generator Set Designed to Meet Tier 4 Final Emission Standards

For Worldwide Release: May 16, 2017
Release Number: EEPR0717

PEORIA, ILL. – Caterpillar Inc. today announced an addition to the company’s line of Tier 4 Final rental power solutions with the introduction of the Cat® XQ125 mobile diesel generator set. Rated at 125 kVA for prime operation, the new product meets Tier 4 Final emission standards while improving fuel efficiency and optimizing productivity over the previous Tier 4 interim package for rental operations in the United States and Canada.

“This new model provides our customers with another option for accessing the right power at the right time,” said Marina Waters, engineering manager with Caterpillar’s Global Power Solutions Division. “The XQ125 has better power density than competitive packages, reducing installation footprint while delivering more reliable, clean power.

Equipped with the sophisticated Cat® Connect platform, the new Cat XQ mobile diesel generator sets combine equipment, technology and services to build customer success. Cat Connect allows the dealer to remotely monitor multiple generator set parameters such as run hours and fuel consumption, through easy-to-use analysis tools. The timely information allows customers to control costs, improve performance and reduce risks.

Complementing the advanced monitoring offering, the Cat XQ125 features the easy to use EMCP 4.2B control panel providing power metering and protective relaying along with engine and generator control and monitoring. The EMCP 4.2B is embedded with Programmable Logic Controller (PLC) functionality, which enables the generator set to monitor and control other equipment within the operation. Each EMCP4.2B includes inputs to collect supplementary data for the PLC to process when operating the generator set and activating external equipment. On a remote location without the ability to supply power to the battery charger, the PLC would likewise monitor the battery voltage to start and stop the machine to preserve battery ensuring the unit is ready to run when needed.

In addition, the Cat XQ125 is powered by a C 4.4 ACERT™ industrial diesel engine offering the perfect balance of durability, efficiency and low emissions. With advanced research and development techniques, the aftertreatment system is precisely matched to the engine ensuring performance is optimized for maximum productivity.

A robust, rental-ready construction allows for easy and efficient transportation around project sites, while a galvanized enclosure protects the XQ125 from potentially harsh environments.

Capable of 500-hour oil change intervals, the XQ125 features increased uptime, lower maintenance costs and consumes fewer parts and oil making it friendlier for the environment.

All Cat XQ mobile generator sets are supported by the Cat® dealer network. Cat dealers are available 24 hours a day, 7 days a week to assist with customer’s emergency rental needs. Caterpillar’s service network ensures access to prompt; quality repairs by trained technicians at Caterpillar authorized service locations.

For more information, visit www.cat.com/rentalpower or e-mail cat_power@cat.com. To interact with other power generation professionals in our online community, register at www.catelectricpowerinfo.com/connect.

 

Available Images

Download here or contact Kellie Mazur at kmazur@gelia.com

Cat® XQ125 Tier 4 Final Mobile Generator Set

Cat XQ125 Tier 4 Final Mobile Generator Set

 

Cat XQ125 Tier 4 Final Mobile Generator Set

 

# # #

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38,5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Power Systems - and also provides financing and related services through its Financial Products segment.  For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow,” the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2017 Caterpillar
All Rights Reserved

 

Press Inquiries

Kellie Mazur 
Gelia
Tel: +1 716-629-3174
kmazur@gelia.com

Michelle Biltimier
Caterpillar Inc.
Tel: +1 309-578-4962
biltimier_michelle_d@cat.com

 

Reader Requests Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610