Caterpillar Launches Cat® 3512C Diesel Generator Set with Improved Power Density for Standby Applications

For Worldwide Release: March 6, 2017
Release Number: EEPR0417

Latest in a series of new ratings for medium to large diesel generator sets ranging from 1,250 kW to 2,800 kW that significantly reduce customer’s installed costs

PEORIA, ILL. – Caterpillar Inc. today announced a new standby power node for the Cat® 3512C diesel generator set that offers industry-leading power density. Rated at 1,750 kW for 60 Hz standby applications, the Cat 3512C generator set offers reliable backup power from an optimally sized engine and a reduced overall footprint that delivers numerous benefits, including lower overall site preparation, transportation, installation and maintenance costs, as well as reduced fuel consumption and lower emissions.

The Cat 3512C diesel generator set is the latest in a series of new ratings for proven standby power solutions from Caterpillar. These generator sets have been re-engineered with the higher power densities requested by customers to meet increasingly challenging restrictions on capital, site size, and cost. Over the next six months, Caterpillar will offer seven new ratings based on existing, proven platforms that deliver the benefits of high power density to our customers around the globe. The full line will feature power nodes ranging from 1,250 kW to 2,800 kW that can significantly reduce customer’s installed costs over current product offerings.

“Maximizing the return on investment for standby power requires customers to specify a solution that is precisely sized to balance power availability and reliability with lower costs,” said Lenaik Andrieux, general manager for Caterpillar’s Large Electric Power Division. “These standby generator sets with improved power densities will allow customers to fine-tune the selection of the power they need through a compact package that can significantly reduce their costs for both the short and long term.”

The Cat 3512C generator set has a highly competitive footprint of 151.56 square feet, saving up to 13 percent of installed space when compared with competing generator sets at the same rating. It is designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. The Cat 3512C generator set also meets ISO 8528-5 G3 requirements for steady state and load acceptance. It can be configured to meet the US EPA Emergency Regulations.

The Cat 3512C generator set can be equipped with a low- or high-voltage frame alternator that enables quick load acceptance through exceptional motor starting capabilities. This feature allows users to minimize oversizing the generator set due to motor starting requirements.

The Cat 3512C generator set utilizes the field-proven Cat ADEM™ A3 engine control module (ECM), which integrates all engine functions including ignition, governing, air-fuel ratio control, and engine protection.

Caterpillar is a leader in the power generation marketplace with power systems engineered to deliver unmatched durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service every aspect of Cat equipment.

For more information, visit www.cat.com/powergeneration or e-mail cat_power@cat.com. To interact with other power generation professionals in our online community, register at http://forums.cat.com/powerperspectives

 

Available Images

Download here or contact Bob Chase at bchase@gelia.com

3512C Diesel Generator Set With Improved Power Density

 

# # #

About Caterpillar

For 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent.  Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets.  With 2015 sales and revenues of $47.011 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives.  The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment.  For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow,” the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2017 Caterpillar
All Rights Reserved

 

Press Inquiries

Bob Chase 
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Chuck Boysen
Caterpillar Inc.
Tel: +1 309-578-4962
Boysen_Charles@cat.com

 

Reader Requests Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610