Cat® Dealer Whayne Power Systems Repowers Three Marathon Petroleum Inland Waterways Vessels

Ashland, Kentucky – When long-time customer Marathon Petroleum wanted to repower inland river towboats, they turned to their trusted Cat® dealer Whayne Power to get the job done. Marathon had installed Cat 3606 engines on the inland waterways vessels in the early 1990s and twenty years later was ready to repower three towboats with the successor to the 3600 engine series, the Cat C280. Starting in December 2013, Whayne Power worked with Marathon to repower the three vessels with Cat C280-6 engines, each rated at 2548 bhp @ 900 rpm.

“Marathon Petroleum has been a proud Cat customer for decades and had great success with the reliability and durability of the Cat 3606 engines since the initial installation of the engines,” Lincoln Turnage, Whayne Power marine account manager noted. “They were impressed with the long overhaul intervals and were eager to repower their vessels with the C280 engines, which have the perfect speed and power fit for their applications on the inland rivers.”

Manufactured in Lafayette, Indiana, Cat C280 engines incorporate 30 years of proven component  reliability and durability from the legendary Cat 3600 platform series with a sophisticated, yet well-proven, modern electronic fuel injection system. Cat C280 marine engines are available in continuous and maximum continuous ratings at 900 and 1000 rpm and in 6, 8, 12, and 16 cylinder configurations The advanced ADEM™ A3 electronic control system enables the C280 engines to work smarter and harder. The rugged and durable C280 engines provide customers with low owning and operating costs, with overhaul intervals running as long as 40,000 hours. “At Whayne, our customers have found the C280 delivers on the same Cat brand promise as the 3606 engines, which developed a long-standing reputation on the waterways as a reliable workhorse,” Turnage noted. “With the increasing demands for the C280 platform on inland waterway applications, we’ve become incredibly proficient at completing comprehensive repowers quickly to get our customers’ vessels back on the water.”

Cat marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. For more information on Caterpillar Marine, visit www.marine.cat.com. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal.

# # #

 

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100  kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: MARINE.CAT.COM/pr

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

Press Inquiries

Jenna Janik Marcoux                                             
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com