Caterpillar Marine to Showcase C7.1, C8.7 and Cat® Marine Displays at the 2017 Yachts Miami Beach Show

Miami, FLCaterpillar Marine is pleased to showcase the Cat® C7.1 Propulsion Engine at the 2017 Yachts Miami Beach show, to be held February 16 – 20, 2017. Cat Marine engines set the standard for quality, performance and reliability—and this new propulsion engine is no exception. Available in three ratings: 507 mhp (373 bkW), 456 mhp (336 bkW) and 406 mhp (298 bkW), all at 2900 rpm, all C7.1 power ratings meet EPA Tier 3, IMO II, EU Recreational Craft Directive and EU Stage IIIA regulations.

The C7.1 is ideal for recreational boating applications, specifically smaller vessels and motoryachts ranging from 25 -60 feet in size. The engine features a common rail fuel system enabling optimum combustion and low emissions. The engines provide noticeably quiet operation due to reduced combustion noise through advanced electronic control. Additionally, no visible smoke is emitted from the C7.1 engines during operation.

Along with the C7.1, Caterpillar Marine will showcase the C8.7 high performance propulsion engine. The C8.7’s sophisticated fuel delivery system allows the use of a radial, belt-driven supercharger in addition to the conventional turbocharger; this feature eliminates smoke and reduces lugging, while delivering phenomenal low-end torque and impressive fuel economy. The electronically-controlled C8.7 is capable of delivering an impressive 650 MHP @ 2300 RPM while meeting EPA Tier 3, IMO 2, EU Stage IIIA and RCD emissions requirements.

In addition to the propulsion engines, the Caterpillar booth at Collins Avenue will be showcasing the CMD (Cat Marine Display) 5 inch, (which will be put into production later this year) CMD 7 inch, and the CMD13 inch displays for the commercial and recreational marine markets. The displays feature intuitive touch screen user navigation, sleek edge to edge glass, optically bonded, anti-glare technology, High Bright performance, IP 66 front & IP 22 rear ratings, and multiple datalinks (2x CAN, 2x Ethernet, 2x USB & 1x RS485). Additionally, these Cat displays include ABS, BV, DNV, GL, LRS, and ClassNK Marine Society Approvals. Stop by the Caterpillar booth to learn about the recent software releases for the CMD7 and the CMD13 displays.

Caterpillar’s Collins Avenue booth will be located at ENT 1-3, be sure to stop by to see the engines, displays and meet the technical experts. In addition to the Yachts Miami Beach show, Caterpillar and Pantropic Cat will be on site at booth #F-407 at the Miami International Boat Show at the Key Biscayne location where they’ll be showcasing a C9 cutaway and an additional C7.1. Follow us on our Facebook page: www.facebook.com/catyachting and Twitter: www.twitter.com/catmarineglobal for up-to-the-minute information on Caterpillar Marine.

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: www.cat.com/marine

About Caterpillar:

For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent.  Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives.  The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment.  For more information, visit caterpillar.com.  To connect with us on social media, visit caterpillar.com/social-media.

©2017 Caterpillar
All Rights Reserved

C7.1 Propulsion Engine
      C7.1 Propulsion Engine

PLEASURE CRAFT MARINE ENGINES

PLEASURE CRAFT MARINE ENGINES

Cat marine engines set the standard for quality, performance and reliability. An extensive power range and decades of experience result in a single source for total power solutions on board, providing electronic marine engines, generator sets, motors and vessel controls.

Learn More

Press Inquiries

Sarah Pullen

Phone: +1 309 675 1513

Pullen_Sarah_C@cat.com