Caterpillar Chosen to Provide 24 ATEX Zone 2 Explosion Proof Packages

For Worldwide Release: May 2014
Release Number: CO&G14PR12

Custom Cat® C15 Air Compressor Package to Be on Display at OTC Houston

Houston, Texas - Caterpillar Oil & Gas is pleased to announce it has been awarded a contract to provide 24x custom Cat® C15 air compressor packages to Airpac Bukom Oilfield Services, a division of Vp plc. Each C15 package is rated at 536 bhp (400 bkW) @ 1800 rpm and the finished package will provide 1600 cfm at 150 psi, while meeting the stringent DNV 2.7-2 certification requirements. Cat dealer Ring Power led the efforts in conjunction with Caterpillar Oil & Gas and Pyroban, a Caterpillar company, to design and develop the compressor packages. The packaging of the units is being completed at Ring Power’s Central Florida location. One of the C15 Air Compressor Packages manufactured for the project will be on display at the Caterpillar booth #3341 at OTC Houston, May 5th – 8th.

“For our customers, our capability to provide ATEX Zone 2 explosion proof packages enables operational flexibility,” Isaac Fox, Caterpillar Oil & Gas Application Engineer noted. “We understand our customers’ needs for integrated safety solutions and are glad we can support their efforts to increase the safety of their operations.”

The C15 custom air compressor units were designed to be compliant with global standards for worldwide usage in a rental fleet. The units feature an air inlet shutoff

as a method of stopping the engine in the presence of a flammable atmosphere and an intake flame arrestor to prevent flames within the intake manifold from spreading to the outside atmosphere. The packages are equipped with water-cooled flexible exhaust pipes with a rugged vibration-resistant design, developed specifically for offshore applications. The exhaust gas heat exchanger in the custom units reduces the temperature of exhaust gas to meet area requirements and has been explosion tested and certified for use in Zone 2 areas.

“Ring Power, Caterpillar and Pyroban have worked hard to develop a solid relationship of teamwork and collaboration through all stages of this project,” said VP Roger Adkins, Ring Power Air Compressor business manager. “Moving forward, Ring Power will continue to train and provide CompEx-certified technicians to support Caterpillar and our customers in the field.”

Cat hazardous location solutions are fully customizable and designed to integrate with complex equipment with offerings ranging from components to complete power solutions and generator sets for a broad spectrum of applications. The hazardous location engine is rated at 536 bhp between 1,800- 2,000 rpm, with an ambient capability of 50° C for the mechanical systems and 60° C on the electrical system.

A variety of hazardous-location certified attachments are available, including an alternator, ATEX Messenger and ATEX throttle control and inlet air flame trap. This engine also features Non-Sparking (nA) and Intrinsically Safe (ic) ECM wiring harnesses and sensors, as well as harness cable jackets that meet flame propagation requirements of IEC 60332-1-2. Having a completely designed, tested and certified package from Caterpillar allows the customer to reduce project complexity and decrease certification-related risks. 

All Cat Oil & Gas products are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. To learn more about the explosion protection packages from Caterpillar or other Cat products, please visit the company’s booth at the 2014 OTC Houston exhibition. For up to the minute information on Caterpillar Oil and Gas at OTC, follow us on Facebook: & Twitter: using #catatotc and #otchouston.

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions that include reciprocating engines, generator sets, transmissions and well stimulation pumps. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations worldwide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at:

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Power Systems - and also provides financing and related services through its Financial Products segment. For more information, visit To connect with us on social media, visit

Press Inquiries
Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449