Caterpillar Introduces Fourth Mobile Generator Set Designed to Meet Tier 4 Final Emission Standards

For Worldwide Release: May 13, 2016
Release Number: EEPR0316

PEORIA, IL – Caterpillar Inc. today announced the expansion of the company’s line of rental power solutions with the introduction of the Cat® XQ60 mobile diesel generator set. Rated at 60 kVA for prime operation, the new product meets Tier 4 Final emission standards while improving fuel efficiency and optimizing productivity for rental operations in the United States and Canada.

The XQ60 is Caterpillar’s fourth Tier 4 Final mobile generator set in the range extending from 35 to 570 kVA. 

“For the latest XQ mobile generator set, we completely refreshed the design focusing on meeting more than just the emission regulations with new features specifically designed for the end user,” says Brian Kruse, general manager at Caterpillar Rental Power. “We were able to reduce the overall package weight allowing the unit to be mounted in a single axle trailer, which provides superior maneuverability when compared to a twin axle trailer. But beyond that, we achieved the Tier 4 Final emissions without the addition of selective catalytic reduction (SCR) and Diesel Exhaust Fluid (DEF).”

Equipped with Caterpillar’s easy to use EMCP 4.2B control panel, the Cat XQ60 includes power metering, protective relaying and engine and generator control and monitoring. The EMCP 4.2B also enhances performance and ease of operation by integrating the voltage regulator and simplifying the process for changing voltage to suit various applications. Multiple distribution options provide additional receptacles for customers to conveniently connect to based-on operation needs. 

A robust, rental-ready construction allows for easy and efficient transportation around project sites, while a smaller footprint saves space and provides installation versatility. The galvanized enclosure protects the XQ60 from potentially harsh environments.

Capable of 500-hour oil change intervals, the XQ60 features increased uptime, lower maintenance costs and consumes fewer parts and oil making it friendlier for the environment.

All Cat XQ mobile generator sets are supported by the Cat dealer network. Cat dealers are available 24 hours a day, 7 days a week to assist with customer’s emergency rental needs. Caterpillar’s service network ensures access to prompt; quality repairs by trained technicians at Caterpillar authorized service locations. 

For more information, visit www.cat.com/rentalpower or e-mail cat_power@cat.com. To interact with other power generation professionals in our online community, register atwww.catelectricpowerinfo.com/connect.

XQ60 Tier 4 Final Mobile Generator Set
XQ60 Tier 4 Final Mobile Generator Set

Image Downloads

XQ60 Tier 4 Final Mobile Generator Set

 

# # #

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.2 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Power Systems - and also provides financing and related services through its Financial Products segment.  For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow,” the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2016 Caterpillar. All Rights Reserved.

Press Inquiries

Kellie Mazur 
Gelia
Tel: +1 716-629-3174
kmazur@gelia.com

Michelle Biltimier
Caterpillar Inc.
Tel: +1 770-233-3938
biltimier_michelle_d@cat.com

Reader Requests Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610