Caterpillar is BUILT FOR IT™ at World of Concrete

For Release in North America: February 2015
Release Number: 63PR15

With decades of innovation and expertise working on the customer’s behalf, Caterpillar is offering a new generation of U.S. EPA Tier 4 Final and E.U. Stage IV engines from 5.5 bhp (4.1 kW) to more than 1200 bhp (895 kW), that meet high expectations for reliability, performance, fuel and fluid efficiency and component life, with significantly reduced emissions. Ours is the largest industrial engine power range of any manufacturer in the industry with the latest technological advancements built on a legacy of quality. Cat® industrial engines are utilized by a wide range of OEMs in construction, mining, and general industrial sectors. No matter what emissions technology your jobsite requires, we have an engine to meet your needs and your equipment’s configuration.

Technologies

Caterpillar has selected from a portfolio of engine and aftertreatment technologies to meet the latest emissions standards, while providing optimum value in each power range. The technology offering includes a diesel oxidation catalyst (DOC), diesel particular filter (DPF) and selective catalytic reduction (SCR). Additionally, a “No DPF” aftertreatment package is available on select platforms.

Expertise

With millions of working hours on thousands of units since the U.S. EPA Tier 4 Interim, E.U. Stage IIIB product introductions, Caterpillar builds on its expertise and proven experience of its Tier 4 Final technology. The entire line of Cat U.S. EPA Tier 4 Final and E.U. Stage IV engines is precisely engineered, rigorously tested and validated, and built for reliability and durability.

Engine line up at World of Concrete 2015

This year Cat industrial engines will exhibit in the Central Hall, booth C6061. The U.S. EPA Tier 4 Final, E.U. Stage IV model featured is the C4.4 ACERT™ power unit. With turbo after-cooled and series turbo configurations, this 4.4 liter, 4 cylinder engine is rated at 100-173.5 bhp (74.5-129.4 kW) and delivers a complete package, providing a simple solution to meeting U.S. EPA Tier 4 Final, E.U. Stage IV emissions standards.

Value

“Caterpillar equips every U.S. EPA Tier 4 Final and E.U. Stage IV engine with a combination of electronic, fuel, air and aftertreatment components based on engine size, the type of application, and the geographic location in which it will work,” says Mike Reinhart, Caterpillar Industrial Regional Marketing Manager.

Serviced by the most extensive dealer network in the world, Cat industrial engines are offered with a comprehensive warranty, financing, and extended service plans which provide customers with the best choice for their most demanding applications. Visit our industrial engine and see for yourself that Caterpillar is BUILT FOR IT™.

###

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission. 

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2015 Caterpillar All Rights Reserved

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas
Sharon Holling: Holling_Sharon_L@cat.com
Johanna Kelly: Kelly_Johanna_L@cat.com

Reader Requests

www.cat.com/requestCatinfo