Caterpillar Marine to power One of the world's largest split hopper dredger with full propulsion solution

Hamburg, Germany – Caterpillar Marine is pleased to announce one of the world’s largest split hopper dredger is being built with a complete Cat® engine and propulsion package. The 4200 cubic meter capacity vessel designed by MARIC Design House in conjunction with the Jiangsu Haixin shipyard, receives its shaft propulsion power from two Cat C280-8 engines which are used to power Cat MTA727 controllable pitch azimuthing thrusters. The electrical load is supplied by generators mounted on the front of the C280-8 engines and backed up by a C32 harbor genset and a C7.1 emergency genset.

The C280-8 provision of mechanical shaft power to the thrusters from the flywheel end and electrical shaft power off the C280-8 front end provides a simplified installation that helps maintain engine efficiency.

The all Cat vessel design allows for a single point of contact for best in class global service and parts support. “The propulsion system is very critical for dredgers in terms of operations and financial returns,” Mr. Jiang Guowang, deputy GM of Jiangsu Haixin Shipyard commented. “The high reliability and power efficiency of Cat engines, combined with Lei Sing Hang’s strong technical and service capability are the main reasons we choose Caterpillar Marine solution.”

The vessel is scheduled for launch in September of 2017

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: www.cat.com/marine

About Caterpillar:

For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent.  Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives.  The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment.  For more information, visit caterpillar.com.  To connect with us on social media, visit caterpillar.com/social-media.

©2017 Caterpillar

All Rights Reserved

 


DREDGE

Dredging plays a vital role in the marine industry, allowing cargo and passenger ships to travel through unobstructed waterways. It’s a tough job, and dredging vessels need engines that deliver reliable performance, high fuel efficiency and best-in-class power.

Read More

Press Inquiries

Sarah Pullen

Phone: +1 309 675 1513

Pullen_Sarah_C@cat.com