Caterpillar Oil & Gas Launches C175-16 IMO Tier II – 1800 rpm Generator Set for Offshore Industry

Houston, TX – Caterpillar Oil & Gas is pleased to introduce industry-leading power with its newest C175-16 IMO Tier II Emissions Certified Generator Set. Rated at 2800 bkW (3755 bhp) / 2660 ekW* @ 1800 rpm, this new generator set has the ability to meet stringent safety requirements for emergency applications or can be adapted to meet main power or essential offshore requirements.

“What’s significant about this product launch is that we’re putting out a higher rated power at 1800 rpm and we’re doing it with fewer cylinders than what our competitors use for similar density,” said Scott Roberts, oil and gas offshore marketing manager for Caterpillar. “Our customers will benefit with less maintenance and lower operating costs due to fewer cylinders, while still getting the new higher rated power.”

The new C175-16 generator set features high pressure electronic unit injection to maximize fuel efficiency and performance while maintaining emission standards. It offers a twenty-five degree static and dynamic tilt capability to handle the toughest environments.

When designing this new generator set, we took into account the limited amount of space our customers have on offshore rigs,” said Roberts. “The overall size and package weight of this unit will be an added benefit to our customers.”

The C175-16 IMO Tier II Emissions Certified generator set is available now for order through the Cat® dealer network. For more information on this product and other solutions for the oil and gas industry, follow Caterpillar Oil & Gas on Facebook (http://www.facebook.com/caterpillaroilandgas), Twitter (http://www.twitter.com/catoilandgas) or learn more on Cat.com.

©2016 Caterpillar
All Rights Reserved

C175-16 Offshore Generator Set

Offshore Solutions Power Ratings

Cat engines are hard at work on the majority of the world’s offshore oil wells. Their robust design, low-speed operation, fuel economy and low overall costs make them the industry’s top choice for offshore drilling power.

Download Ratings

Press Inquiries

Sarah Pullen

Phone: +1 309 675 1513

Pullen_Sarah_C@cat.com

Jenna Janik Marcoux                                             

Phone: +1 713 895 1449

Marcoux_Jenna_J@cat.com