Caterpillar Selected by Keppel FELS to Power Five Super B Class Jackup Rigs

Caterpillar Oil & Gas announced today that the Cat® C175 and Cat 3516B generator sets have been selected to power five high spec Super Class B jackup rigs. Each rig will be equipped with five Cat C175 generator sets, each with rated power of 1833 ekW @ 60 Hz (1200 rpm), for prime power as well as 1x Cat 3516B generator set providing emergency power. The newbuilds are currently being constructed by Keppel FELS in Singapore and the Cat power solutions will be delivered over the course of the next two years. Cat dealer Tractors Singapore Limited (TSL) led Caterpillar’s efforts on the project.

“Cat dealer TSL has delivered outstanding support to Keppel FELS since the Cat C175 power solutions were selected in a previous Super Class B order in 2011 and we’re pleased to continue to collaborate with Keppel FELS on jackup newbuilds,” Shen Yang Lee, Caterpillar Oil & Gas Asia Pacific territory sales manager for ASEAN region noted. “The Cat C175 is the industry leader for jackup rigs in the offshore industry, reliably powering jackup rigs operating around the globe drilling at varied depths.”

The Cat C175 is ideal for customers seeking high power density, high fuel efficiency, and minimized downtime in offshore drilling applications. Offering 20 percent more installed power than 3516C (HD) offshore generator sets, the C175-16 allows for deeper drilling and higher mud pump loading. Its compact footprint offers significant weight savings when compared to medium speed engines and allows for retrofit with today’s Cat 3516 generator sets.  In addition, its full featured control system provides for easy interface with the local rig network, and can be controlled and monitored remotely.

The C175-16 is also highly fuel efficient, incorporating a fuel system that uses a high pressure fuel pump and control valve that deliver multiple precise injections within a single combustion event. This results in lower emissions, improved performance and reduced fuel consumption. Driven by two ADEM™ A4 engine control modules, the C175-16 engine features full redundancy and provides superior performance, even in the most demanding environments. The fuel system directly impacts customers overall owning and operating costs as the fuel consumption has been optimized for typical drilling load.

For more information on the solutions and services Caterpillar Oil & Gas offers, please visit Follow us on Facebook: & Twitter:

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions that include reciprocating engines, generator sets, transmissions and well stimulation pumps. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations worldwide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at:

About Caterpillar

For more than 85 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company also is a leading services provider through Caterpillar Financial Services, Caterpillar Remanufacturing Services and Progress Rail Services. More information is available at:

More information is available at

Press Inquiries
Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449