Caterpillar Selected by Longzhu Oilfield Services to power Jackup Rigs for FTS Derricks

Beijing, China - Caterpillar Oil & Gas announced today that the Cat® C175-16 and Cat C32 generator sets have been selected by Longzhu Oilfield Services (S) Pte Ltd to power four jackup newbuilds in China for FTS Derricks Pte Ltd, a subsidiary of Falcon Energy. Five Cat C175-16 generator sets, each with rated power of 1930 bkW at 1200 rpm, will be used as the prime power for each jackup while 1x Cat C32 generator set providing emergency power. The newbuilds are currently under construction at Shanhaiguan Shipyard in China and the units will be delivered over the course of the next 2 years. Cat dealer WesTrac China led Caterpillar’s efforts on the project. The Cat C175-16 generator set will be on display at the Caterpillar booth at the 2014 CIPPE Show, March 19th – 21st in Beijing, China.

“The Cat C175-16 generator set is the power solutions of choice for offshore jackup rigs in the region,” Tim Tian, Caterpillar Oil & Gas Asia Pacific - China dealer sales territory manager noted, “Along with the reliable power of the Cat C175-16, Cat dealer Westrac China has been able to deliver outstanding service and support to both the customer and the shipyard.”

The Cat C175-16 is ideal for customers seeking a high power density and lower emissions offshore drilling module. Offering 20 percent more installed power than previous models, the Cat C175-16 allows for deeper drilling and higher mud pump loading. Its compact footprint offers significant weight savings when compared to medium speed engines and allows for retrofit with today’s Cat 3516C HD module design.  In addition, its full featured control system provides for easy interface with the local rig network, and can be controlled and monitored remotely.

The Cat C175-16 is also highly fuel efficient, incorporating a fuel system that uses a high pressure fuel pump and control valve that deliver multiple precise injections within a single combustion event. This results in lower emissions, improved performance and reduced fuel consumption. Driven by the ADEM™ A4 controller, the Cat C175-16 engine management system features full redundancy and provides superior performance, even in the most demanding environments. The fuel system directly impacts customers overall owning and operating costs as the fuel consumption has been optimized for typical drilling load.

All Cat Oil & Gas products are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. To learn more about these or other Cat products, please visit the company’s booth at the 2014 CIPPE Beijing event, Hall W1, Booth W1503.  For more information, visit

For up to the minute information on Caterpillar Oil and Gas, follow us on Facebook: & Twitter:


Image 1

# # #

About Caterpillar Oil & Gas
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW.  The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at:

About Caterpillar
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit To connect with us on social media, visit

Press Inquiries
Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449