Caterpillar Sells First Cat® C280 Generator Set into China Offshore Market

For Worldwide Release: Mar 2015
Release Number: CO&G15PR3

Beijing, China - Caterpillar Oil & Gas announced today that Cat® C280-16 offshore generator sets have been selected to power a BT-4000 Light Workover semi-submersible for the Brazilian oil service contractor, Etesco.  Six Cat C280-16 generator sets rated at 5500 ekW (6111 kVA) @ 60 Hz (900 rpm) will power the semi-submersible and it will be built at DSIC Offshore, one of China’s leading turnkey EPC contractors for offshore construction, for delivery in 2016. The milestone sale marks the entrance of the legendary Cat C280 power solution into China offshore market and all six generator sets will be delivered to DSIC Offshore in September 2015.  Cat dealer, WesTrac China Limited, led Caterpillar’s efforts on the project for this major win.   

“The Cat C280-16 engine has an outstanding reputation as a reliable power solution, logging countless hours in the engine rooms of offshore rigs around the globe” Alan Zhang, Caterpillar Oil & Gas Asia Pacific China region sales manager, noted. “We’re pleased to introduce this quality product to the China market where it will undoubtedly achieve the superb performance benchmarks that it is noted in deepwater drilling applications.”

The maximum continuous rating of 5500 ekW positions the Cat C280-16 as the most power dense offshore generator set of its class. A long-standing industry workhorse, the IMO II compliant Cat C280 offers optimized fuel consumption engineered specifically for drilling applications. Manufactured in Lafayette, Indiana, Cat C280 is equipped with   ADEM™ A4 ECM as well as Cat Alarm and Protection System providing customers with enhanced remote monitoring capabilities and an innovative control system to detect potential safety issues. The ease and speed of installation on the rig is increased due to the front-mounted turbocharger and integration of peripheral parts and systems into the package.

For more information on the solutions and services Caterpillar Oil & Gas offers, please visit http://www.catoilandgasinfo.com/pr. Caterpillar Oil & Gas industry experts will also be on hand at the 2015 CIPPE Show. Please stop by the Caterpillar booth in Hall W1, Booth W1503 to meet with one of our industry professionals.

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW.  The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow”, the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2015 Caterpillar
All Rights Reserved

 

Press Inquiries

Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449
Marcoux_Jenna_J@cat.com