Caterpillar to Feature the Latest in Engine Technologies at the 15th CIPPE Exhibition in Beijing, China

For Worldwide Release: Mar 2015

Beijing, China – Caterpillar Oil & Gas will unveil its latest innovative power solutions developed specifically for the Chinese oil and gas market at the 15th China International Petroleum and Petrochemical Technology and Equipment Exhibition (CIPPE) from March 26th to 28st  in Beijing, China. Launching at this year’s exhibition is Cat® 3512C HD Land Electric-Drive Drilling Module which meets China Stage III Non-Road Mobile Emissions (6.4 NOx+HC, 3.5 CO, 0.2 PM g/kW-hr). Cat 3512C platform in 1045 ekW (60 Hz) @ 1200 rpm rating will be on display at the Caterpillar booth.

“At CIPPE 2015, we are highlighting our broad range of trusted power solutions for Asia Pacific with several new products developed specifically the region and its customers,” said Alan Zhang, Caterpillar Oil & Gas Asia Pacific China region sales manager.  “We’re pleased to feature Solar Turbines, a subsidiary of Caterpillar Inc, at our booth for the first time and commemorate forty years of Caterpillar operations in China this year!”

Also on display at the Caterpillar booth at the 2015 CIPPE Exhibition include:

  •          The Cat 3512B Land Electric Drilling Module with Dynamic Gas Blending (DGB):
    The Cat 3512B Generator Set with DGB offers customers fuel flexibility without sacrificing performance and is available in a 1245 ekW (1750 kVA) @ 50 Hz (1500 rpm) rating. The Dynamic Gas Blending kit automatically adjusts to changes in incoming fuel quality and pressure allowing engines to run on a wide variety of fuels, from associated gas to vaporized LNG with no loss of performance integrity. It maintains diesel performance levels with up to 70 percent replacement of diesel with gas, accepts up to 55 percent inerts. No customer input or gas analysis is needed during operation, and no recalibration is required when the equipment is moved or the gas supply changes.
  •          TH55-E70 Transmission – The TH55-E70 transmission is optimized for petroleum pumping applications. Its evenly spaced gear ratios provide smooth shifting for pumping, providing for a much broader range of pumping speeds than the competition. The transmission with 7 speed option and deep first gear ratio creates application flexibility, and allows pumping at lower flow rates and pressure.
  •          Scale Model of GenSet ATEX Zone 2: A detailed scale model of an explosion proof Generator Set suitable for safe operation in Zone 2 hazardous areas, will be displayed on the stand, demonstrating the complexity of explosion proofing equipment. Pyroban, a Caterpillar company, offers ATEX Zone 2 explosion proof packages, fully customizable and designed to integrate with complex equipment with offerings ranging from components to complete power solutions and generator sets for a broad spectrum of applications. In addition to explosion proof packages, Pyroban offers a range of Ex products including up-fit kits for existing engines.

For more information on the solutions and services Caterpillar Oil & Gas offers, please visit http://www.catoilandgasinfo.com/pr. Caterpillar Oil & Gas industry experts will also be on hand at the 2015 CIPPE Show, held March 26 – 28th in Beijing, China. Please stop by the Caterpillar booth in Hall W1, Booth W1503 to meet with one of our industry professionals.

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW.  The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

More information is available at www.cat.com.

About Solar Turbines

Headquartered in San Diego, California, USA, Solar Turbines Incorporated, a subsidiary of Caterpillar Inc., is one of the world’s leading manufacturers of industrial gas turbines, with more than 15,000 units and over 2 billion operating hours in 100 countries.  Products from Solar Turbines play an important role in the development of oil, natural gas and power generation projects around the world. Solar Turbines’ products include gas turbine driven compressor sets, mechanical-drive packages and generator sets (ranging from 1-22 megawatts). 

In China, Solar has sold over 300 units for both onshore and offshore applications including electric power, gas transmission, export compression offshore, and gas gathering.  Solar Turbines (Beijing) Service Trading & Services Co. Ltd. was established in Year 2011, and now has over 50 employees in China. Products include gas turbine product families, Saturn®, Centaur®, Mercury™, Taurus™, Mars®, Titan™, and a line of centrifugal gas compressors including both pipeline and production compressors. Solar also manufactures Turbotronic™ microprocessor-based control systems utilizing PLC technology.  Solar offers total life cycle support for all products worldwide including parts, services, refurbishments, and overhauls.  More information is available at https://mysolar.cat.com

 

Press Inquiries

 

Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449
Marcoux_Jenna_J@cat.com