Caterpillar to Launch New Cat® CG137-8 Generator Set at the 2014 Williston Basin Petroleum Conference

Houston, TX – Caterpillar Oil & Gas is pleased to unveil the new Cat® CG137-8 natural gas generator set at the 2014 Williston Basin Petroleum Conference, held May 20 – 22nd at the Bismarck Civic Center in Bismarck, North Dakota. The new Cat CG137-8 generator set provides 282 ekW (352 kVA), 60 Hz @ 1800 rpm of rated power, offering customers an additional power node to complement existing Cat power solutions in land production applications. The CG137-8 generator set is now available to order from the global Cat dealer network.

“The CG137-8 generator  set power node is a great addition to the proven Cat G3306B (135 ekW) and CG137-12 (400 ekW) oilfield generator sets, Russ Goss, Caterpillar Oil & Gas  new product introduction project manager said. “This range of offerings and their tolerance of high BTU-content fuels provide customers the ability to select the ideal amount of power required for their unique applications.”

The Cat CG137-8 is a V8, 4-stroke-cycle generator set offering fuel flexibility enabling operation on a wide range of gas quality – from wellhead gas to pipeline quality natural gas. The generator set features superior gas engine transient capability as well as the ADEM™ A4 control system providing integrated ignition, speed control, and engine protection. Both the component design and fuel flexibility allow minimum site preparation and low installation cost. The generator set is NSPS site compliant capable when configured with customer-supplied air-fuel ratio control and a three-way catalyst.

Cat dealers Butler Cat and Tractor & Equipment Company will both have booths showcasing Cat oil & gas offerings at the Willison Basin Petroleum Conference. Both dealers proudly serve and support the growing North Dakota oilfields. On display at the Butler Cat booth (#12 & 13) will be the first Cat CG137-8 generator set manufactured as well as the Cat WS273XD, a 2700 bhp triplex pressure pump. Tractor & Equipment Company will be exhibiting at booth #307.

“Caterpillar is uniquely suited to power North Dakota oilfields not only with our rugged land drilling, production and pumping solutions but also through the superior capabilities of the Cat dealers in the territory, Butler Cat and Tractor & Equipment Co.,” Aaron Jenkins, Caterpillar Oil & Gas territory sales manager noted. “The Williston Basin Petroleum Conference is a great opportunity for both current and potential customers to come and see the solutions that can be customized for their local operations.”

The Cat WS273XD is a triplex well stimulation pump with 2700 bhp (2014 bKW) input power and 275 maximum rpm. The complete Cat well stimulation pump product portfolio consists of four well stimulation pumps in triplex and quintuplex configurations in a standard, Extreme Duty (XD) series or Stainless Steel (SS) series. The Cat well stimulation pumps feature fluid ends and power ends designed to an industry standard footprint, allowing customers to easily fit the Cat pump into their existing trailer designs.  In addition to the standard fluid ends, Caterpillar offers an XD fluid end with superior durability for the harshest operating conditions as well as stainless steel fluid ends which are compatible with all Cat XD series components.

Cat power solutions are sold and fully supported through the global Cat dealer network. For more information on the solutions and services Caterpillar Oil & Gas offers, please visit Follow us on Facebook: & Twitter:

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions that include reciprocating engines, generator sets, transmissions and well stimulation pumps. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations worldwide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at:

About Caterpillar

For more than 85 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company also is a leading services provider through Caterpillar Financial Services, Caterpillar Remanufacturing Services and Progress Rail Services. More information is available at:

More information is available at

Image 1

Press Inquiries
Caterpillar Oil & Gas Press Relations:
Jenna Janik Marcoux
Tel: +1.713.895.1449