Caterpillar Unveils New Cat® Displays for Yachts at the 2014 Miami International Boat Show

Miami, FL – Caterpillar Marine is pleased to announce the launch of the next generation color marine power displays for customers in the yacht market segment. The 7” and 13” displays will be entering the market in late 2014, and they will feature multi-touch capable screens, user friendly swipe navigation, Home Button, and improved graphics. These displays will be fully integrated with the Cat marine engines and Cat Three60 propulsion solutions. The 13” inch Cat display will be featured with the Cat Three60 Precision controls simulator at the Caterpillar booth #P79 at the Miami International Boat Show, held February 13-17th in Miami, Florida.

“We’re very excited to introduce our new, top-of-the-line touch screen displays with Linux Operating System,” Merritt Callaghan, Caterpillar Marine Electronics supervisor said. “We’ve worked closely with our process partners to develop a market leading display suited to the unique marine market requirements.”

The Cat display was designed to integrate seamless with the high-end yacht bridges. It will feature low bezel height, optical bonded glass for optimized daylight readability, viewable with polarized lens, LED backlight, multiple datalinks (2x CAN, 2x Ethernet, 2x USB & 1x RS485), and external output drivers for audible alarms. The new Cat displays will include ABS, BV, DNV, GL, LRS, and ClassNK Marine Society Approvals. Additionally, the 13” inch display will be a future service replacement for the existing Cat Engine Vision displays.

Display software will support standard Cat marine display features plus, modern graphics, optimized day and night modes with an auto-dimming feature, swipe navigation between multi operator screens, multiple Ethernet cameras, a real time clock, external USB keyboard/mouse support and PDF file uploads. Additionally, it will feature enhanced Three60 Precision features like Station Keeping Activation, Station Keeping GPS position, Three60 diagnostics, Shaft Speed and Bow/Stern thruster percent activation.

“The new Cat displays will undoubtedly enhance our customers experience with their Cat power solutions and maximize the ease of vessel operation on the water,” Chad McIntosh, Caterpillar Marine Product Definition engineer noted.

For more information on the new Cat displays, please visit the Caterpillar booth #P79 at the upcoming Miami International Boat Show and speak with one our industry professionals. Unable to make the show? Follow us on follow us on Twitter: and Facebook: using #catatmia.

# # #

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat® and MaK marine engines within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: MARINE.CAT.COM/pr

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Power Systems - and also provides financing and related services through its Financial Products segment. For more information, visit To connect with us on social media, visit

©2014 Caterpillar

All Rights Reserved

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Press Inquiries
Jenna Janik Marcoux
Phone: +1 713 895 1449
Cell: 979-541-9997