Confidence in MaK™ Dual Fuel Conversions

Caterpillar continues to be successful in MaK™ Dual Fuel engine retrofits & supplies complete gas system for Fure West Tanker

Hamburg Germany – Building on the success of recent MaK diesel engine dual fuel retrofit conversions, Caterpillar Marine is currently underway on another dual fuel engine retrofit conversion onboard the 472 foot Fure West tanker, owned by Furetank Rederi A/B. The MaK™ M 43 C diesel engine onboard the tanker will be retrofitted in hull to the 7 cylinder M 46 dual fuel platform, with each cylinder offering 900 kW of rated power. Additionally, Caterpillar is also supplying the complete gas system for the tanker, including bunker stations, 2x LNG tanks measuring 4.15 meters by 24 meters and the vaporizer.

This project, backed by the European Union and developed with the Zero Vision Tool, will mark the second MaK engine dual fuel retrofit. In 2014, Caterpillar successfully completed the dual fuel engine retrofit conversion on the Anthony Veder Coral Anthelia LNG carrier. “We’re pleased to continue to build upon our successful track record of dual fual conversions in the commercial marine industry and offer an increased scope of supply to our customers,” Finn Vogler, Caterpillar Marine senior engineer noted. “We have a market-ready technology available that our commercial marine customers can be completely confident in and after our success onboard the Coral Anthelia, we have seen the demand for MaK dual fuel solutions increase substantially.”

With a bore of 460 millimeters and stroke of 610 millimeter, the M 46 dual fuel engine was designed for electric drive propulsion systems as well as mechanical propulsion systems. Although designed for unlimited operation on LNG, marine diesel oil and heavy fuel oil, the M 46 DF will reach industry-leading efficiency in gas mode. The M 46 DF was strategically engineered to allow for the retrofitting of current M 43 C engines. Additionally, existing M 32 E engines can be retrofitted to the MaK M 34 DF dual fuel platform. As a result of the synergies between the two platforms, Caterpillar can perform in hull retrofit conversions without having to move the engine block or perform extensive machining. For the Fure West conversion, Cat dealer Pon Power had a significant role in the project. “We’re able to differentiate our solutions in the market by offering a collaborative partnership with our dealers to ensure the retrofit conversions are completed in an expedited manner and with a reduced number of parties involved as a result of our ability to provide the complete gas system for a vessel as well,” Vogler noted.

Cat marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. For more information on Caterpillar Marine, visit www.marine.cat.com. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal.

# # #

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: www.cat.com/marine

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

More information is available at www.cat.com.

Press Inquiries

Jenna Janik Marcoux                                             
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com

 


Marine Selection Guide

No matter the application or solution, we have what you need. Our Cat, MaK & EMD products are renowned for not only reliability, durability and efficiency, but also for design & manufacturing innovation. Our mission is to be a total provider of advanced marine power systems & services with the highest uptime and lowest cost of ownership.

Download the Guide

MaK M 46 DF Dual Fuel Propulsion Engine

The low emission footprint paired with high efficiency and reliability make the M 46 DF an ideal propulsion engine for operation, inside and outside of environmental protected areas as well as waters with HFO limitations.

Learn More