Custom Cat® C15 Air Compressor Package to be on display at OTC Houston

Houston, Texas - Caterpillar Oil & Gas will display a custom Cat C15 Air Compressor package in an enclosure configuration at the 2015 OTC Houston Show, held May 4th – 7th in Houston, Texas.  Each C15 package is rated at 536 bhp (400 bkW) @ 1800 rpm and the finished package will provide 1600 cfm at 150 psi, while meeting the stringent DNV 2.7-2 certification requirements. Cat dealer Ring Power led the effort to design and develop the custom compressor packages in conjunction with Caterpillar Oil & Gas, Pyroban, a Caterpillar company, and Sullair Corporation. Ring Power will soon be offering additional Cat-powered models: 250 cfm, 400 cfm and 1000 cfm. The custom packages are offered in both skid and enclosed configurations. Ring Power is the first Cat dealer building air compressor packages to DNV 2.7-2 requirements

“Ring Power and our partners have worked hard to develop a solid relationship of teamwork and collaboration through all stages of this project,” said Roger Adkins, Ring Power Air Compressor vice president. “Moving forward, Ring Power will continue to train and provide CompEx-certified technicians to support Caterpillar Oil & Gas and our customers in the field.”

The C15 custom air compressor units were designed to be compliant with global standards for worldwide usage in a rental fleet. The units feature an air inlet shutoff as a method of stopping the engine in the presence of a flammable atmosphere and an intake flame arrestor to prevent flames within the intake manifold from spreading to the outside atmosphere. The packages are equipped with water-cooled flexible exhaust pipes with a rugged vibration-resistant design, developed specifically for offshore applications. The exhaust gas heat exchanger in the custom units reduces the temperature of exhaust gas to meet area requirements and has been explosion tested and certified for use in Zone 2 areas.

Cat hazardous location solutions are fully customizable and designed to integrate with complex equipment with offerings ranging from components to complete power solutions and generator sets for a broad spectrum of applications. The hazardous location engine is rated at 536 bhp between 1,800- 2,000 rpm, with an ambient capability of 50° C for the mechanical systems and 60° C on the electrical system.

A variety of hazardous-location certified attachments are available, including an alternator, ATEX Messenger and ATEX throttle control and inlet air flame trap. This engine also features Non-Sparking (nA) and Intrinsically Safe (ic) ECM wiring harnesses and sensors, as well as harness cable jackets that meet flame propagation requirements of IEC 60332-1-2. Having a completely designed, tested and certified package from Caterpillar allows the customer to reduce project complexity and decrease certification-related risks.

All Cat Oil & Gas products are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. To learn more about the explosion protection packages from Caterpillar or other Cat products, please visit the company’s booth at the 2015 OTC Houston exhibition. For up to the minute information on Caterpillar Oil and Gas at OTC, follow us on Facebook: http://www.facebook.com/caterpillaroilandgas  & Twitter: http://www.twitter.com/catoilandgas using #catotc and #otchouston.

 

Print Media

# # #

About Caterpillar Oil & Gas

Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

More information is available at www.cat.com.

Press Inquiries  
     
Jenna Janik Marcoux
Phone: +1 713 895 1449
Cell: +1 979 541 9997
Marcoux_Jenna_J@cat.com