Pantropic Cat® Charges New Life into Aging Vessels

It’s inevitable – engines have to be replaced eventually. The repowering process can be daunting, and one that vessel owners put off, but Pantropic Cat’s experience in repowering vessels makes it an option worth considering. With a robust Authorized Marine Dealer (AMD) network and access to proven technology like the C32 engine, Pantropic Cat® is making it easier than ever to update your power.

Pantropic’s eight AMDs are located throughout the South Florida region, and they are all highly skilled at replacing older Cat® (or other branded) engines with newer, cleaner, more reliable technology and iron.  The presence of AMDs allows Pantropic to expedite repowering and servicing, often reducing downtime by weeks. These AMDs follow the same rigorous standards that all Cat dealers are held to—it’s like having access to nine service centers instead of one.

Repowering makes the most sense for owners of pleasure craft and commercial vessels, including barges, dredges and container boats. Prior to repowering, Pantropic assesses the owner’s needs for their vessel, whether it is increasing the vessel’s speed, efficiency or addressing some other concern. The repowering process is also an ideal time for vessel owners to service additional vessel systems, as Pantropic’s AMDs can perform any needed maintenance, even if it’s just laying on some new paint.

Although Pantropic can install a wide range of Cat Marine engines, it is the C32 that stands out for its impressive array of features. The C32 is an ideal replacement for older two-stroke engines that many older vessels are fitted with. The shift to the C32 will mean increased fuel efficiency, lower emissions, better reliability and quieter operations while increasing overall lifespan. Transitioning from a two-stroke to a newer model will improve parts availability as well, ensuring service is faster and more affordable. Finally, the C32 is lighter than competing engines and offers a wider operating speed range, driving efficiency and power up even further.

Stop by the Caterpillar / Pantropic booth #F407 the Miami International Boat Show, Key Biscayne Island location. Caterpillar will be showcasing a C9 cutaway and C7.1 propulsion engine, in addition to having experts on hand to talk about why a Cat re-power engine is right for you.

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: www.cat.com/marine

About Caterpillar:

For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent.  Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives.  The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment.  For more information, visit caterpillar.com.  To connect with us on social media, visit caterpillar.com/social-media.

 

©2017 Caterpillar

All Rights Reserved


PLEASURE CRAFT MARINE ENGINES

Learn more Caterpillar Marine in the Recreational Boating and Yachting industry.

Learn More

Press Inquiries

Sarah Pullen

Phone: +1 309 675 1513

Pullen_Sarah_C@cat.com