Cat® Grade Control 3D for D3K2, D4K2, and D5K2 Models Boosts Productivity, Lowers Costs, and Reduces Operator Effort

For Release in North America, Europe, Australia, New Zealand, Japan, Korea: November 2016 
Release Number: 498PR16

Cat® Grade Control 3D, by automating machine functions during both production-dozing and fine-grading applications, enables dozer operators to work more efficiency, accurately, and productively, while also lowering operating costs. The system features an integrated design, including dual, roof-mounted antennas that eliminate the need to climb onto the blade to remove conventional blade-mounted masts and cables at the end of the day. The AccuGrade™ Ready Option is part of the package, adding versatility by allowing other Cat GRADE technologies to be used, such as AccuGrade Laser or a universal total station when satellite reception is limited.

The system assists operators with an in-cab display that shows grade plan, cut/fill data, and grade indicators, improving productivity up to 50 percent, compared with conventional grading methods. The system virtually eliminates the need for staking and manual grade checking, making the job site safer and allowing the operator to work unassisted to move material exactly as required—saving rework, fuel, and machine wear. In addition, Grade Control 3D allows work to proceed even in limited visibility, extending the work day. As an added benefit, the system's automated blade control reduces required operator input by as much as 80 percent.

The integrated design of the Grade Control 3D system, in addition to the roof-mounted antennas, features an inertial measurement unit that senses machine orientation, GNSS (Global Navigation Satellite System) receivers, data radio, position-sensing hydraulic cylinders, joystick buttons for rapid grade adjustments, and a full-color grade-control display that visually indicates grading progress. In addition, the system includes three “intelligent" operating features that allow the machine to match blade loads with ground conditions, resulting in consistently full blades with reduced operator effort.

AutoCarry™— automates blade lift and pitch to maintain desired blade load, improve load consistency, and reduce track slip.

Complementing the automated implement-assist feature are three modes that further assist the operator in working productively. Working as an integrated system, these technologies can significantly reduce overall costs by producing more work, in less time, with a subsequent reduction in machine operating costs.

Grade Control—automates blade lift and tilt for consistent grades and optimizes productivity with AutoCarry.

Rough Grade—prevents downward movement of the blade center below grade, permitting full tilt-steer capability.

Grade Protection—prevents the blade from cutting below the target grade during manual blade operation, reducing overcutting.

Grade Control 3D further allows site managers to automatically track material movement and monitor job progress via the system's 3D track mapping data. Timely information encourages timely decisions that keep work on schedule. Production data can be viewed daily via Cat LINK technologies by using the online VisionLink® 3D Project Monitoring capability, which does require a subscription and additional hardware.

The Grade Control 3D system is available for D3K2, D4K2, and D5K2 models and is supported by local Cat dealers and SITECH® technology partners.

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2016 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests www.cat.com/requestCatinfo