Cat® M-Series Small Wheel Loaders, 930M Ag Handler Deliver with Performance-Enhancing Upgrades

For Release in North America: November 2016
Release Number: 520PR16

Recent engineering enhancements to the U.S. EPA Tier 4 Final Cat® M Series Small Wheel Loaders (SWL) – 926M, 930M and 938M, as well as the K Series models (924K, 930K, 938K) – advance equipment value through new standard and optional features that boost productivity, improve operating ease and increase uptime reliability. Additionally, the Ag segment-specific solution incorporates new features to increase the payload capacity, hydraulic speeds and flow pressures demanded by agricultural customers.                                      

Upgraded Secondary Display

A new secondary display module option for all models within the product line improves operator interface and navigation, and it makes available a host of special payload management and service options. The new touchscreen display features a QWERTY keyboard, making it easier for the owner/operator to navigate through the menu and input text like coded start operator profiles, application profiles, service-mode and preventative maintenance alerts. The new display significantly reduces the amount of time for information entry and eliminates the arrow keys required by previous versions for navigation and data inputting. 

Caterpillar Production Measurement

A first for the Cat small wheel loader models, adding the touchscreen display and Product Link Elite to these small loaders ushers in the availability of Caterpillar Production Measurement. The management system’s tip-off capability confirms to the operator that there is sufficient weight in the bucket before leaving the pile, increasing machine productivity. When this Cat feature is active on a 924K, 926M, 930K, 930M, 938K or 938M, it gives the operator the ability to place the proper amount of material in the feed wagon, mixer, hopper or truck the first time, every time, reducing the number of cycles and maximizing profit potential.

Caterpillar Production Measurement allows the operator to set target loading weight and monitor the cumulative amount of material loaded into a truck or hopper, which helps to prevent overloading. Additionally, the available system printer gives the operator the ability to print up to three copies of a recorded weight ticket. Since Caterpillar Production Measurement is fully integrated into the machine, the site manager can track important statistical information like amount of material moved and number of trucks loaded with the use of VisionLink®.          

Increased Machine Reliability

Enhancements to Cat Auto-Lube include the replacement of rubber hoses and swivel joints with steel lines running to the bucket pins, improving system durability. New secondary zerks added to the system enable the operator to manually grease circuits, should the need arise. To save time, the technician can add grease quickly to the new main manifold, which greases every circuit on the loader, or specific individual circuits can be greased independently.

Auto-Lube is fully integrated into the new secondary display and Cat VisionLink, which automatically sends diagnostic codes to the operator and designated key personnel like fleet managers to help with troubleshooting. Should the grease reservoir run low or other system issue arises, a pop-up banner is shown on the secondary display notifying the operator of the problem, so it can immediately be addressed. 

To increase tire longevity, Tire pressure monitoring (TPM), a first to market, is now a fully integrated option for the M Series small wheel loader machines. With a quick glance at the secondary display, the operator can easily see current tire pressures for each tire, ensuring they are properly inflated to reduce uneven wear and maximize tire life. The system can be configured to provide warnings to dealers through Electronic Technician and the operator via the secondary display if tire pressures drop too low or increase too high. Since TPM is a fully integrated system, fleet managers can use VisionLink to track air pressuring and temperature in each machine from a remote location for optimal machine performance and efficiency.

Comfort and Power

The updated deluxe operator’s cab design offers a new standard binder/clipboard storage area for securely storing papers and manuals, while an extra 1.2 ft3 (0.03 m3) of lockable storage can be optionally mounted to the bottom side of the cab for securing tools, grease guns, gloves and other items. Climate controlled with heated rear glass and external mirrors for rapid defrost, the quiet cab design boasts seat-mounted controls featuring a low effort joystick for lift and tilt functions.

The M Series SWL machines are powered by the Cat C7.1 ACERT™ engine with clean emissions module that requires no operator intervention, which avoids work cycle disruptions. The operator has the option of selecting standard mode operation that reduces maximum engine speed to 1,600 rpm without compromising peak ground performance, resulting in a 5 to 10 percent fuel savings. Full performance mode operation boosts engine speed to 1,800 rpm for maximum engine power and increased hydraulic speed and power to boost production. 

Specially Designed Ag Handler*

Designed with increased payload, faster cycle times and higher hydraulic power, the Cat 930M Ag Handler efficiently meets the needs of the agricultural market. Offering a 50 gal/min hydraulic flow rate, this Ag handler delivers 20 percent faster cycle times compared to standard M Series SWL models. The 930M Ag Handler also offers increased payloads with right-sized high lift, which delivers 2,490 lb. (1,129 kg) more tip load compared to the 926M high lift and 1,480 lb. (671 kg) higher than the standard 930M high lift. Its 12 percent higher pressure, coupled with increased higher flow, delivers more hydraulic power to get the most out of hydro-mechanical tool attachment operation, such as the silage defacer. 

*The 930M Ag Handler will only be available in North America.

 

M Series SWL Product Specifications

 

926M

930M

938M

Engine

Cat C7.1 ACERT

Cat C7.1 ACERT

Cat C7.1 ACERT

Net Power – Standard (ISO 9249)

142 hp (106 kW)

156 hp (116 kW)

169 hp (126 kW)

Operating Weight

28,770 lb.
(13,050 kg)

30,879 lb.
(14,007 kg)

36,216 lb.
(16,427 kg)

3rd Hydraulic Flow

150  L/min (40 gpm)

190  L/min (50 gpm)

190  L/min (50 gpm)

4th Hydraulic Flow

150  L/min (40 gpm)

160 L/min  (42 gpm)

160  L/min (42 gpm)

Fusion general purpose bucket capacity

2.7 yd3 (2.1 m3)

3.0 yd3 (2.3 m3)

3.5 yd3 (2.7 m3)

Full turn tipping load

16,587 lb. (7 524 kg)

18,670 lb. (8 469 kg)

22,107 lb. (10 028 kg)

Maximum travel speed

25 mph (40 km/h)

25 mph (40 km/h)

25 mph (40 km/h)

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2016 Caterpillar All Rights Reserved

Contact presse

Représentants Caterpillar auprès de la presse spécialisée

Continent américain

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Afrique, Moyen-Orient

Francine Shore: Shore_Francine_M@cat.com

Contact www.cat.com/requestCatinfo