Cat® MD5150C Top Hammer Drill proves performance in tough applications

For Release Worldwide: February 2015
Release Number: 79PR15

Even in granite-like conditions the new Cat® MD5150C Top Hammer Drill is out-performing down-the-hole rigs with its higher productivity and much lower fuel consumption—while achieving comparable hole straightness. Cat drill customer Iron Mountain Quarry, located south of St. Louis, Missouri, USA, reports that overall productivity is almost double a competitor’s DTH drill. This productivity is achieved with the powerful Cat HPR6832 hydraulic rock drill, the new carousel rod changer and the efficient Cat C11 Engine.

Beyond feet per minute, the cost per foot is a clear winner, too. At Iron Mountain, the MD5150C

drills 5.5-inch (140-mm) diameter holes to 70 ft (21.33 m) deep using 68-mm-diameter drill rod, commonly called drill steel. The bit can last 1,100 to 1,200 ft (335 to 366 m), which is the same consumption rate as the previous down-the-hole drill. Fuel consumption, on the other hand, is much less than the competitor’s DTH drill. Further, the drill steel experiences less wear and long life. Owning and operating cost for the Cat machine is lower with the simple rock drill design, which can be serviced in the field.

According to Matt Jacobs, Cat Drills Commercial Manager, “We saw similar results in an earlier trial at a Tower Rock limestone quarry near St. Genevieve, Missouri.  That site has softer rock conditions and the MD5150C dramatically outpaced a competitor’s DTH drill. Austin Powder conducted a bore tracking test and the results showed a hole deviation rate with the MD5150C Top Hammer Drill that was within the desired range. Tower Rock Quarry was very pleased with its higher production and lower operating cost—all while achieving similar hole straightness.”

Consistent production results in both hard and soft rock demonstrate the capability of the new Cat MD5150C Top Hammer Drill. All Cat drills are supported by the Cat Dealer network, which offers unparalleled capabilities to keep Cat machines running productively and efficiently.

 

Print Media

# # #

Additional media:

Link to testimonial video: https://www.youtube.com/watch?v=rPh1TCQ8-b8

Link to 360 Degree virtual product tour: http://www.cat.com/en_US/products/new/equipment/drills/track-drills/18563259.html

 

Press Inquiries

Caterpillar Trade Press Media Representatives
Americas
Sharon Holling: Holling_Sharon_L@cat.com
Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East
Francine Shore: Shore_Francine_M@cat.com
General Email: Cat_Trade_Press@cat.com

 

Reader Requests

 

www.cat.com/requestCatinfo