Cat® Launches Rigid Frame Truck Bare Chassis for Specialty Applications

For Worldwide Release: September 22, 2012

Release Number: 298PR12

Cat® 785D WTR, 777G WTR, 775G WTR and 773G WTR Truck Bare Chassis for Specialty Applications

Caterpillar now offers bare chassis configurations of several Cat® Off-Highway and Mining Trucks for the increasingly important water truck market.  The WTR configurations are available for the Cat 785D Mining Truck, 777G, 775G and 773G Off-Highway Trucks (Tier 4 certified and Tier 2 equivalent). 

The WTR configurations have unique standard and optional attachments specific to specialty applications like water trucks.  For example, they can be ordered with or without hoist cylinders.  The ROPS structure on the WTR chassis is certified to the ISO 3471 Tractor rating.  And beginning January 1, 2013, the 777G WTR chassis can be ordered with the optional Cat Water Delivery System.

NOTE:  The WTR configurations can be utilized as the base machine for tow tractor applications; however, the entity converting this configuration to a tow tractor will need to ensure that the finished product meets applicable requirements for roll over protective structure (“ROPS”), braking, steering, sound limitations, operating performance, weight limitations, etc.  As sold by Caterpillar, the WTR chassis configurations are certified as rigid frame hauling units only. 

Cat® Dealers can order WTR configurations through their normal machine order channels.  The Cat Dealer or end-user customer is responsible for purchasing the water tank from a variety of tank manufacturers around the world who can also assemble the tank onto the chassis.  Caterpillar OEM Solutions Group has engineering resources to assist with water tank, water delivery system and control integration.

Following are tables of suggested tank sizes and weight limits by WTR configuration:

Water Tank Size

Model*

L (gal) - Approximate

Less

773G WTR

45 400 – 49 200 (12,000 – 13,000)

Less

775G WTR

56 750 – 64 340 (15,000 – 17,000)

Less

777G WTR

68 100 – 75 700 (18,000 – 20,000)

Less

785D WTR

113 562 (30,000)

Less

*Tier 4 certified and Tier 2 equivalent.

Targeted Gross Machine Operating Weight

Model*

kg (lb)

Less

773G WTR

102 740 (226,503)

Less

775G WTR

111 812 (246,503)

Less

777G WTR

164 654 (363,000)

Less

785D WTR

 249 476 (550,000)

Less

*Tier 4 certified and Tier 2 equivalent.

 

# # #

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

Downloadable Images

Press Inquiries

Cat Trade Press Media Representatives

Americas
Sharon Holling: Holling_Sharon_L@cat.com
Christina Schave: Schave_Christina_M@cat.com

Europe, Africa, Middle East
Francine Shore: Shore_Francine_M@cat.com

General Email: Cat_Trade_Press@cat.com

Reader Requests
www.cat.com/requestCatinfo

Cat rigid frame truck
Rigid frame truck bare chassis for specialty applications