Cat® Wheeled Excavators and Wheel Material Handlers Receive Blue Angel Environmental Certification

For Release in Europe, Israel, Americas North, Puerto Rico, Australia, New Zealand: November 2016 
Release Number: 523PR16

The Blue Angel certification is an environmental award— supported by the German Federal Environmental Agency and the Federal Ministry for the Environment, Nature Conservation, Building and Nuclear Safety— that recognizes products that protect both people and the environment by reducing noise and emissions. The Cat® M318F, M320F, and M322F wheeled excavators and the MH3022 and MH3024 wheel material handlers have been awarded this coveted certification in recognition of the Caterpillar commitment to environmental protection. The Cat 906M, 907M, 908M, 926M, 930M, and 938M wheel loaders were previously awarded Blue Angel certification.

Blue Angel certification

The Cat models were tested for Blue Angel certification in the construction machinery category for sound and emission levels, by RAL GmbH, the German Institute for Quality Assurance and Certification. Granting the Blue Angel label is based on the methodology used in the statutory procedures, and at the same time, takes into account state-of-the art technology for the reduction of exhaust, particle, and noise emissions. The requirements and test values are more stringent than statutory limits for the European Union. Today, Caterpillar is the only manufacturer to have received the Blue Angel certification in the construction machinery category for its products.  

Cat F Series

When designing the F Series wheeled excavators and material handlers, Caterpillar solicited the guidance of both product experts and customers—those who use these machines on a day-to-day basis and know first-hand what characteristics are important. Safety and environmental considerations were defined as key requirements to give customers not only the exceptional performance they expect from Cat products, but also added value. In addition, these new models feature low operating costs, simplicity of operation, ease of maintenance, and a comfortable operator's station.

 F Series wheeled excavators and the MH3022, MH3024 material handlers use the Cat C7.1 ACERTTM engine that meets EU Stage IV and U.S. EPA Tier 4 Final emission standards. The engine integrates an emission aftertreatment system that imposes no requirements on the operator and functions without interrupting the work cycles.

Environmental enabler

Environmental considerations are becoming crucial in today’s world to help build a more sustainable future. Increasingly, cities and states are implementing access restrictions based on equipment sound and particulate emission levels. The Blue Angel label can be an enabler for customers to work in such areas and is the best guarantee that customers will be well positioned to take on this work with their Cat equipment. Frederic Predemoiser, wheeled excavator global product application specialist, comments “This certification complements our strategy to offer our customers versatile products in all application tasks through a wide range of solutions, integrated technologies, and work tools.”

 

Blue angel, M318F wheeled excavator
M318F wheeled excavator

Specifications

Models

M318F, M320F, M322F

MH3022, MH3024

Engine

C7.1 ACERT

C7.1 ACERT

Net power

(hp metric and kW)

171 (126)

171 (126)

Operating weight

 

17,930 to 24,700 kg

39,529 to 54,454 lb.

20,705 kg/45,646 lb. to

27,470 kg/60,560 lb. (with work tool)

###

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission. 

©2016 Caterpillar All Rights Reserved

 

Print Media

Placeholder image


Download High Resolution Image

M318F wheeled excavator

 

Placeholder image


Download High Resolution Image

M322F wheeled excavator

 

Placeholder image


Download High Resolution Image

MH3024 wheel material handler

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_M@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

General Email: Cat_Trade_Press@cat.com

Reader Requests www.cat.com/requestCatinfo