Caterpillar Adds New High-Production B-Series Tandem Rollers to the Paving Products Machine Family

For Release in North America: November 2015
Release Number: 235PR15

Caterpillar Inc. announces the addition of the new high-production B-Series Tandem Vibratory Rollers that include the CB64B, CB66B, and CB68B models. These machines are 12 to 14 metric ton compactors that feature wider drum widths, high-flow water spray system, increased operator comfort, and enhanced technology to help operators and machines perform at higher levels. Many of the technological enhancements are offered through Cat® Compaction Control. They include Auto-Adjustable Compaction (AAC), Pass-Count and Temperature Mapping, Machine to Machine Communication, and Compaction Meter Value (CMV).

Auto-Adjustable Compaction (AAC)

Simple operation and optimized compaction help contractor’s lower costs. Auto-Adjustable Compaction optimizes compaction by delivering the highest amplitude possible without de-coupling or over-compacting. The technology includes both the front drum and rear drum – a Cat Exclusive. This unique system is able to adjust through the full range of amplitudes in as little as 4 seconds for excellent performance and uniform compaction throughout the mat.

Pass-Count and Temperature Mapping

Pass-Count and Temperature Mapping systems provide real-time visual references of the passes made and asphalt mat temperatures present. Distractions, fatigue, multi-tasking, and nighttime operation can affect how well an operator executes the rolling pattern on an asphalt mat.

Where did I stop on the previous pass? Did I go back far enough on the return pass? Did I provide enough overlap on the previous pass? Is the mat temperature too hot, too cold? These are just a few questions that operators may have throughout the day. By utilizing Cat Compaction Control technology, second-guessing can be eliminated.

Machine to Machine Communication

This system helps keep rolling patterns in sync by sharing coverage and pass-count maps between the operating displays of multiple machines. By viewing the color display, operators can monitor areas of coverage and the number of passes made. If a trailing operator sees an area of missed coverage, they can easily pick it up to ensure the entire rolling pattern gets the attention that is needed. This system is extremely helpful when performing echelon compaction when multiple machines are executing five or seven pass rolling pattern.

Compaction Meter Value (CMV)

CMV technology uses a drum-mounted accelerometer to measure and record forces of the vibrating drums. A calculation derived from the recorded forces is used to create a unit-less value that provides an indication of stiffness. This unit-less value calculation is referred to as a “composite stiffness value” that indicates stiffness of the current and supporting layers beneath the drum. The system is capable of utilizing RTK level accuracy to provide the highest level of Global Navigation Satellite System positioning (GNSS) and is able to correlate compaction, frequency, and pass-count data to specific location.

Efficient Power and Eco-Mode

The Cat C4.4 ACERT™ engine meets U.S. EPA Tier 4 Final and EU Stage IV emissions and provides 106 kW (142 hp) of power. Automatic Eco-mode operates at a variable engine speed to deliver excellent fuel economy and lower sound levels.

Keeping Operators Productive

Visibility and comfort are enhanced by the standard 180º seating and optional 360º positioning. New handwheel steering technology eliminates the front steering console, enabling the operator to easily monitor water spray performance. An LCD display and push-button controls simplify operation for an all-around comfortable operating environment.

Smooth, Maneuverable

These models feature a newly designed center-articulating hitch with 6 degrees of oscillation that ensures mat contact and a smoother ride over uneven surfaces. An offset hitch option extends coverage up to 170 mm (6") and simplifies control next to obstacles. It delivers excellent performance on longitudinal joints by pinching the edge with the lead drum and sealing the joint with the trailing drum.

The CB64B is equipped with 2.0 m (79") drums, while the CB66B and CB68B utilize 2.1 m (84") drums. The Cat C4.4 engine rated at 106 kW (142 hp) comes standard with Eco-mode and automatic speed control, leading to uniform compaction, fuel savings, reduced sound levels, and ultimately lower operating costs.

Versatile Vibratory Systems

The B-Series tandem rollers offer a variety of vibratory options including dual amplitude, dual frequency, Versa Vibe™, and five amplitude systems. The Versa Vibe™ system creates a 2-in-1 machine with four amplitudes and two frequencies. This versatile system provides two settings for lighter hitting and higher working speeds on thin lifts; and two settings for heavier hitting, and slower speeds, on thick lifts or those with challenging mixes. The five-amplitude system offers the widest range of amplitudes with a single frequency.

Durable Water Spray System

Reliable water spray systems are needed to keep rollers on the mat and on pace with the paver. The high-capacity system on these models are designed with dual spray bars, dual pumps, triple filtration, adjustable intermittent operation, and an optional freeze protection kit.

The dual pumps provide back-up capability and alternate with the direction of travel to maximize service life. Clogging is prevented through filters at the fill point, water pumps and spray nozzles. The adjustable intermittent mode conserves water and minimizes re-fills for optimal efficiency. The optional freeze protection kit helps ensure the roller is ready when you need it. 

###

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2015 Caterpillar All Rights Reserved 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Reader Requests www.cat.com/requestCatinfo