2013 ISRI Convention and Exposition

April 9-13, 2013

Orlando, FL

At ISRI 2013, Caterpillar is pleased to launch the new Cat® MH3049 and MH3059 wheeled material handlers. These new machines are the first in the new MH3000 series line of large wheeled material handlers being introduced in the greater than 25 metric ton size class. Other machines on display are the Cat® 938K Small Wheel Loader and 906H2 Compact Wheel Loader and work tools, including the BA22 Broom and the GSH22B Orange Peel Grapple.

Cat Material Handlers

2013 ISRI Convention and Exposition
MH 3049 Material Handler