Caterpillar Introduces G3516C Land Drilling Power Module

For Worldwide Release: September 2013
Release Number: GP13PR22

New Genset to Feature Increased Power, Improved Performance

Houston, TX – Caterpillar Global Petroleum is pleased to introduce the Cat® G3516C generator set for global land drilling applications. Available in early 2014, G3516C offers an increased power rating of 1,555 eKW (2,175 hp) @ 1800 rpm. This next generation drilling module features improved performance at low engine loads and maintains a compact footprint comparable to diesel power modules used in drilling applications today.

“The new Cat G3516C highlights Caterpillar’s continued to commitment to bringing innovative, natural gas solutions to the oil and gas industry,” Stefanie Acosta, Caterpillar Global Petroleum product definition manager noted. “Strategically our goals are to deliver the right product to improve our customers’ performance in the oilfield and the G3516C will enable customers to drill with more power without sacrificing efficiency in operations, size, or weight.”

Manufactured in Lafayette, Indiana the new G3516C is based on the proven G3516 genset platform, which has been powering oilfield drilling applications for over eight years. Along with improved power capability and optimized footprint, the G3516C will also be EPA Spark-Ignited Non-Road Mobile certified upon availability in spring 2014. The G3516C has been engineered to offer improved transient response, fuel tolerance and altitude/ambient capability to maximize product flexibility for various drilling applications. Each of these product performance improvements will be demonstrated during field testing at customer sites throughout early 2014.

The G3516C will be showcased at the upcoming High Horsepower Summit in Chicago, September 17 – 19th where Caterpillar will highlight its comprehensive dual fuel and natural gas offerings for the oil and gas, rail, marine and mining industries. To register for HHP, visit: www.cat.com/hhpsummit. For up to the minute information on Caterpillar Global Petroleum at HHP, follow us on Facebook: http://www.facebook.com/caterpillaroilandgas & Twitter: http://www.twitter.com/catoilandgas using #HHPSummit and #natgas.

For more information on the comprehensive dual fuel and natural gas solutions Caterpillar offers, please visit catoilandgasinfo.com or contact your local Cat dealer.

# # #

About Caterpillar Global Petroleum
Caterpillar Global Petroleum, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, groups all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com/pr

About Caterpillar
For more than 85 years, Caterpillar Inc. has been making progress possible and driving positive and sustainable change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is a technology leader and the world’s leading manufacturer of construction and mining equipment, clean diesel and natural gas engines and industrial gas turbines. More information is available at www.cat.com.

Press Inquiries Caterpillar Press Relations:
Jenna Janik
Tel: +1.713.895.1449
Janik_Jenna_E@cat.com