Caterpillar to Launch EPA Tier 4 Solutions at the International Workboat Show

For Worldwide Release: October 2013
Release Number: M9PR13

Tier 4 Certified Cat® 3500 and C280 Marine Engines Available to Order

New Orleans, LA - Caterpillar Marine Power Systems will unveil a significant product milestone at the 2013 International Workboat Show, introducing its comprehensive United States EPA Tier 4 power solutions for vessels using engines over 2,000 kW. The first engine platforms to be rolled out as Tier 4 solutions are two legendary performers in the commercial marine industry: the Cat® 3516C marine engine as well as the Cat 280 marine engine. The C280 engine will be available as Tier 4 certified in both the 8 and 12 cylinder configurations. The Cat 3516C Tier 4 certified engine as well as the Cat C280-8 Tier 4 certified engine and Cat C280-12 Tier 4 certified engine are now all available for customers to order through the global Cat dealer network.

"Our message to customers is simple: we're ready; come and see us," Mark Harrison, Caterpillar engineering manager stated. "We recognize the emissions regulations impacting the commercial marine industry are both significant and challenging and we want to be present in our customers' decision-making process and work together to design Tier 4 solutions for their vessels. We'll get this done together."

The Cat 3516C Tier 4 certified engine will be available in ratings of 2240 bkW and 2350 bkW @1800 rpm. An auxiliary or diesel electric propulsion solution is available in a 2250 ekW   (2368 bkW) rating.  The Cat C280-8 Tier 4 certified marine propulsion engines will be available in ratings of 2460 bkW and 2710 bkW @1000 rpm with the auxiliary engines and diesel electric propulsion generator set available of 2185ekW and 2400ekW @900 rpm. The Cat C280-12 Tier 4 certified marine propulsion engines will be available in ratings of 3700bkW and 4060bkW @1000 rpm with the auxiliary engines and diesel electric propulsion generator set available ratings of 3320kW and 3640ekW @900 rpm.

Caterpillar Tier 4 marine technology utilizes aftertreatment combined with a fuel efficiency optimized engine to meet the low NOx regulations. Both the C280 and 3516C Tier 4 certified solutions employ selective catalyst reduction (SCR) technology, which will provide customers with the lowest possible owning and operating costs. The SCR module was designed with the engine room in mind with compact dimensions. Additionally the inclusion of SCR technology enables customer to leverage shared components as well as a similar engine footprint to EPA Tier 2 and Tier 3 engines. Harrison noted, "We designed our Tier 4 solutions with one goal in mind: to provide the lowest overall owning and operating costs for our customers. We are aware of the impact the regulations have on our customers' bottom line and wanted to ensure our Tier 4 solutions minimized the costs of adopting this new technology."

The Cat 3516C and C280 Tier 4 certified marine power solutions are ideal for customers in the tug and salvage and offshore industries.  Additional Tier 4 compliant platforms will be launched in the near future.

For more information on Caterpillar Tier 4 solutions for the marine industry or to order a Tier 4 certified power solution, please stop by the Caterpillar booth #2802 at the upcoming Workboat Show, December 9th - 11th in New Orleans, LA. Industry experts will be on hand, readily available to answer any questions. For up to the minute updates at the show, please follow us on Twitter: https://twitter.com/catmarineglobal and Facebook: https://www.facebook.com/caterpillarmarine using #catatwbs.

# # #

About Caterpillar Marine Power Systems
Caterpillar Marine Power Systems, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine engines within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100  kWe in marine generator sets. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are. More information is available at: MARINE.CAT.COM/pr

About Caterpillar
For more than 85 years, Caterpillar Inc. has been making progress possible and driving positive and sustainable change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is a technology leader and the world's leading manufacturer of construction and mining equipment, clean diesel and natural gas engines and industrial gas turbines. More information is available at www.cat.com.

Press Inquiries
Jenna Janik Marcoux 
Phone: +1 713 895 1449
Janik_Jenna_E@cat.com